RAIL_SyncWordConfig_t Struct Reference

RAIL sync words and length configuration.

#include <rail_types.h>

Data Fields

uint8_t syncWordBits
 Sync word length in bits, between 2 and 32, inclusive.
 
uint32_t syncWord1
 Sync Word1.
 
uint32_t syncWord2
 Sync Word2.

RAIL sync words and length configuration.

Definition at line 2246 of file rail_types.h.

Field Documentation

◆ syncWordBits

uint8_t RAIL_SyncWordConfig_t::syncWordBits

Sync word length in bits, between 2 and 32, inclusive.

Definition at line 2248 of file rail_types.h.


The documentation for this struct was generated from the following file:
  • common/rail_types.h