#################################################################### # Makefile # # OS variable must either be 'posix' or 'win'. E.g. 'make OS=posix'. # Error is thrown if OS variable is not equal with any of these. # #################################################################### .SUFFIXES: # ignore builtin rules .PHONY: all debug release clean #################################################################### # Definitions # #################################################################### # uniq is a function which removes duplicate elements from a list uniq = $(strip $(if $1,$(firstword $1) \ $(call uniq,$(filter-out $(firstword $1),$1)))) PROJECTNAME = throughput_tester OBJ_DIR = build EXE_DIR = exe LST_DIR = lst #################################################################### # Definitions of toolchain. # # You might need to do changes to match your system setup # #################################################################### RMDIRS := rm -rf RMFILES := rm -rf ALLFILES := /*.* NULLDEVICE := /dev/null SHELLNAMES := $(ComSpec)$(COMSPEC) # Try autodetecting the environment: Windows ifneq ($(SHELLNAMES),) QUOTE :=" ifeq (,$(filter $(OS),posix win)) OS:=win endif ifneq ($(COMSPEC),) ifeq ($(findstring cygdrive,$(shell set)),) # We were not on a cygwin platform NULLDEVICE := NUL endif else # Assume we are making on a Windows platform # This is a convenient place to override TOOLDIR, DO NOT add trailing # whitespace chars, they do matter ! SHELL := $(SHELLNAMES) RMDIRS := rd /s /q RMFILES := del /s /q ALLFILES := \*.* NULLDEVICE := NUL endif # Other than Windows else ifeq (,$(filter $(OS),posix win)) OS:=posix endif endif # Create directories and do a clean which is compatible with parallell make $(shell mkdir $(OBJ_DIR)>$(NULLDEVICE) 2>&1) $(shell mkdir $(EXE_DIR)>$(NULLDEVICE) 2>&1) $(shell mkdir $(LST_DIR)>$(NULLDEVICE) 2>&1) ifeq (clean,$(findstring clean, $(MAKECMDGOALS))) ifneq ($(filter $(MAKECMDGOALS),all debug release),) $(shell $(RMFILES) $(OBJ_DIR)$(ALLFILES)>$(NULLDEVICE) 2>&1) $(shell $(RMFILES) $(EXE_DIR)$(ALLFILES)>$(NULLDEVICE) 2>&1) $(shell $(RMFILES) $(LST_DIR)$(ALLFILES)>$(NULLDEVICE) 2>&1) endif endif CC = gcc LD = ld AR = ar #################################################################### # Flags # #################################################################### INCLUDEPATHS += \ -I../common/uart \ -I../../../../protocol/bluetooth/ble_stack/inc/common \ -I../../../../protocol/bluetooth/ble_stack/inc/host # -MMD : Don't generate dependencies on system header files. # -MP : Add phony targets, useful when a h-file is removed from a project. # -MF : Specify a file to write the dependencies to. DEPFLAGS = \ -MMD \ -MP \ -MF $(@:.o=.d) override ASMFLAGS += \ -std=c99 # Add -Wa,-ahld=$(LST_DIR)/$(@F:.o=.lst) to CFLAGS to produce assembly list files override CFLAGS += \ -fno-short-enums \ -Wall \ -c \ -fmessage-length=0 \ -std=c99 \ $(DEPFLAGS) # Linux platform: if _DEFAULT_SOURCE is defined, the default is to have _POSIX_SOURCE set to one # and _POSIX_C_SOURCE set to 200809L, as well as enabling miscellaneous functions from BSD and SVID. # See usr/include/fetures.h for more information. # # _BSD_SOURCE (deprecated since glibc 2.20) # Defining this macro with any value causes header files to expose BSD-derived definitions. # In glibc versions up to and including 2.18, defining this macro also causes BSD definitions to be # preferred in some situations where standards conflict, unless one or more of _SVID_SOURCE, # _POSIX_SOURCE, _POSIX_C_SOURCE, _XOPEN_SOURCE, _XOPEN_SOURCE_EXTENDED, or _GNU_SOURCE is defined, # in which case BSD definitions are disfavored. Since glibc 2.19, _BSD_SOURCE no longer causes BSD # definitions to be preferred in case of conflicts. Since glibc 2.20, this macro is deprecated. # It now has the same effect as defining _DEFAULT_SOURCE, but generates a compile-time warning # (unless _DEFAULT_SOURCE is also defined). Use _DEFAULT_SOURCE instead. # To allow code that requires _BSD_SOURCE in glibc 2.19 and earlier and _DEFAULT_SOURCE in glibc # 2.20 and later to compile without warnings, define both _BSD_SOURCE and _DEFAULT_SOURCE. # # OSX platform: _DEFAULT_SOURCE is not used, instead _DARWIN_C_SOURCE is defined by default. ifeq ($(OS),posix) override CFLAGS += \ -D_DEFAULT_SOURCE \ -D_BSD_SOURCE endif # NOTE: The -Wl,--gc-sections flag may interfere with debugging using gdb. override LDFLAGS += #################################################################### # Files # #################################################################### C_SRC += \ ../../../../protocol/bluetooth/ble_stack/src/host/gecko_bglib.c \ main.c \ app.c \ # this file should be the last added ifeq ($(OS),posix) C_SRC += ../common/uart/uart_posix.c else ifeq ($(OS),win) C_SRC += ../common/uart/uart_win.c endif s_SRC += S_SRC += LIBS = #################################################################### # Rules # #################################################################### C_FILES = $(notdir $(C_SRC) ) S_FILES = $(notdir $(S_SRC) $(s_SRC) ) #make list of source paths, uniq removes duplicate paths C_PATHS = $(call uniq, $(dir $(C_SRC) ) ) S_PATHS = $(call uniq, $(dir $(S_SRC) $(s_SRC) ) ) C_OBJS = $(addprefix $(OBJ_DIR)/, $(C_FILES:.c=.o)) S_OBJS = $(if $(S_SRC), $(addprefix $(OBJ_DIR)/, $(S_FILES:.S=.o))) s_OBJS = $(if $(s_SRC), $(addprefix $(OBJ_DIR)/, $(S_FILES:.s=.o))) C_DEPS = $(addprefix $(OBJ_DIR)/, $(C_FILES:.c=.d)) OBJS = $(C_OBJS) $(S_OBJS) $(s_OBJS) vpath %.c $(C_PATHS) vpath %.s $(S_PATHS) vpath %.S $(S_PATHS) # Default build is debug build all: debug debug: CFLAGS += -O0 -g3 debug: $(EXE_DIR)/$(PROJECTNAME) release: $(EXE_DIR)/$(PROJECTNAME) # Create objects from C SRC files $(OBJ_DIR)/%.o: %.c @echo "Building file: $<" $(CC) $(CFLAGS) $(INCLUDEPATHS) -c -o $@ $< # Assemble .s/.S files $(OBJ_DIR)/%.o: %.s @echo "Assembling $<" $(CC) $(ASMFLAGS) $(INCLUDEPATHS) -c-o $@ $< $(OBJ_DIR)/%.o: %.S @echo "Assembling $<" $(CC) $(ASMFLAGS) $(INCLUDEPATHS) -c -o $@ $< # Link $(EXE_DIR)/$(PROJECTNAME): $(OBJS) $(LIBS) @echo "Linking target: $@" $(CC) $(LDFLAGS) $^ -o $@ clean: ifeq ($(filter $(MAKECMDGOALS),all debug release),) $(RMDIRS) $(OBJ_DIR) $(LST_DIR) $(EXE_DIR) endif # include auto-generated dependency files (explicit rules) ifneq (clean,$(findstring clean, $(MAKECMDGOALS))) -include $(C_DEPS) endif