Public Attribute Documentation#
status#
uint8_t status
Scanning Status 
 0 - disable 
 1 - enable 
scan_type#
uint8_t scan_type
Scanning type 
#define SCAN_TYPE_ACTIVE 0x01 
#define SCAN_TYPE_PASSIVE 0x00 
filter_type#
uint8_t filter_type
To filter incoming advertising reports 
FILTERING_DISABLED = 0 (default) 
ACCEPTLIST_FILTERING = 1 Note
In order to allow only acceptlisted devices, need to add bd_addr into acceptlist by calling rsi_ble_addto_acceptlist() API
own_addr_type#
uint8_t own_addr_type
Address type of the local device 
#define LE_PUBLIC_ADDRESS 0x00 
#define LE_RANDOM_ADDRESS 0x01 
#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02 
#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03 
scan_int#
uint16_t scan_int
Scan interval 
This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan. 
Range: 0x0004 to 0x4000 
scan_win#
uint16_t scan_win
Scan window 
The duration of the LE scan. LE_Scan_Window shall be less than or equal to LE_Scan_Interval 
Range: 0x0004 to 0x4000