You are viewing documentation for version:2.10.2Public Attributes#uint8_tip_versionuint8_tsocket_iduint8_tlengthuint8_toffsetuint8_tdest_portuint8_tipv4_addressuint8_tipv6_addressunion rsi_rsp_socket_recv_s::@12dest_ip_addruint8_tend_of_the_datauint8_tmore_data_pendingPublic Attribute Documentation#ip_version#uint8_t ip_version[2]socket_id#uint8_t socket_id[2]length#uint8_t length[4]offset#uint8_t offset[2]dest_port#uint8_t dest_port[2]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]dest_ip_addr#union rsi_rsp_socket_recv_s::@12 dest_ip_addrend_of_the_data#uint8_t end_of_the_datamore_data_pending#uint8_t more_data_pending