Public Attributes#

uint8_t
uint8_t
uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

BD Address of the remote device


local_irk#

uint8_t local_irk[16]

16 byte irk of the local device


remote_irk#

uint8_t remote_irk[16]

16 byte irk of the remote device


remote_ediv#

uint16_t remote_ediv

remote device ediv value


remote_rand#

uint8_t remote_rand[16]

remote device rand value


remote_ltk#

uint8_t remote_ltk[16]

remote device ltk value


Identity_addr_type#

uint8_t Identity_addr_type

Identity address type - public/random
0x00 --> Public Identity Address
0x01 --> Random (static) Identity Address
All other values Reserved for future use


Identity_addr#

uint8_t Identity_addr[6]

Identity address which is resolved after security keys exchange


dev_addr_type#

uint8_t dev_addr_type

Device address type