You are viewing documentation for version:2.11.1Public Attributes#uint8_tdev_addruint16_tMaxTxOctetsuint16_tMaxTxTimeuint16_tMaxRxOctetsuint16_tMaxRxTimePublic Attribute Documentation#dev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]Device address of the remote device. MaxTxOctets#uint16_t MaxTxOctetsMaximum Tx Octets to be transmitted MaxTxTime#uint16_t MaxTxTimeMaximu Tx time to transmit the MaxTxOctets MaxRxOctets#uint16_t MaxRxOctetsMaximum Rx Octets to be received MaxRxTime#uint16_t MaxRxTimeMaximum Rx time to receive the MaxRxOctets