Public Attribute Documentation#
pkt_type#
uint8_t pkt_type
Type of the event received from the remote device 
RSI_BLE_WRITE_CMD_EVENT 0x01 
RSI_BLE_WRITE_REQUEST_EVENT 0x02 
RSI_BLE_NOTIFICATION_EVENT 0x03 
RSI_BLE_INDICATION_EVENT 0x04 
att_value#
uint8_t att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro