Public Attributes#
Public Attribute Documentation#
transmit_enable#
uint8_t transmit_enable
Enables/disables the ble per transmit mode 
1 PER Transmit Enable 
0 PER Transmit Disable 
phy_rate#
uint8_t phy_rate
Phy rate at which packets are transmitted 
 1 1Mbps 
 2 2 Mbps 
 4 125 Kbps Coded 
 8 500 Kbps Coded 
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening. 
In order to enable, one should give the scrambler seed value which is used on the receive side 
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel) 
 0x00 Advertise Channel 
 0x01 Data Channel (to be used by Default) 
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used 
 0 No Hopping 
 1 Fixed Hopping 
 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode) 
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna. 
 2 ONBOARD_ANT_SEL 
 3 EXT_ANT_SEL 
rf_type#
uint8_t rf_type
Selection of RF type (internal/external) 
 BIT[7:6] - RECT selection for BLR (Default value -> 0b00) 
 BIT[5:4] - RECT selection for BLE 2 Mbps (Default value -> 0b00) 
 BIT[3:2] - RECT selection for BLE 1 Mbps (Default value -> 0b00) 
 BIT[1:0] - for rf_type(external - 0/internal - 1) (Default value -> 0b01) Note
The above macros are applicable for BLE
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used 
 2 BT_HP_CHAIN 
 3 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
pkt_len#
uint8_t pkt_len[2]
Length of the packet to be transmitted Max pkt_len to be transmitted is 255
payload_type#
uint8_t payload_type
Type of payload data sequence 
 0x00 PRBS9 sequence �11111111100000111101... 
 0x01 Repeated �11110000� 
 0x02 Repeated �10101010� 
 0x03 PRBS15 
 0x04 Repeated �11111111� 
 0x05 Repeated �00000000� 
 0x06 Repeated '00001111' 
 0x07 Repeated '01010101' 
tx_power#
uint8_t tx_power
Transmit Power 
 This field corresponds to the transmit power. The range for the Tx Power Index is 1 to 63 (0 and 32 are invalid.) 
 If rf chain is BT_HP_CHAIN 
 1 - 12 BLE - HP Mode 
 127 magic number for selecting maximum possible power output 
 If rf chain is BT_LP_CHAIN 
 1 - 31 BLE - 0 dBm Mode 
 33 - 63 BLE- 10 dBm Mode 
transmit_mode#
uint8_t transmit_mode
Transmit mode to be used either Burst/Continuous 
 0 BURST_MODE 
 1 CONTINUOUS_MODE 
 2 CONTINUOUS_WAVE_MODE (CW_MODE) 
inter_pkt_gap#
uint8_t inter_pkt_gap
This field takes the value of inter packet gap. 
Number of slots to be skipped between two packets - Each slot will be 1250usec 
num_pkts#
uint8_t num_pkts[4]
This field defines the number of packets to be transmitted, default to zero for continuous transmission