Public Attribute Documentation#
maxtxoctets#
uint16_t maxtxoctets
maxtxoctets 
 Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection. 
maxtxtime#
uint16_t maxtxtime
maxtxtime 
 Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection 
maxrxoctets#
uint16_t maxrxoctets
maxrxoctets 
 Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection 
maxrxtime#
uint16_t maxrxtime
maxrxtime 
 Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.