Public Attribute Documentation#
cfg_enable#
uint8_t cfg_enable
Definition at line 1673
of file include/rsi_wlan.h
opermode#
uint8_t opermode[4]
Definition at line 1674
of file include/rsi_wlan.h
feature_bit_map#
uint8_t feature_bit_map[4]
Definition at line 1675
of file include/rsi_wlan.h
tcp_ip_feature_bit_map#
uint8_t tcp_ip_feature_bit_map[4]
Definition at line 1676
of file include/rsi_wlan.h
custom_feature_bit_map#
uint8_t custom_feature_bit_map[4]
Definition at line 1677
of file include/rsi_wlan.h
band#
uint8_t band
Definition at line 1678
of file include/rsi_wlan.h
scan_feature_bitmap#
uint8_t scan_feature_bitmap
Definition at line 1679
of file include/rsi_wlan.h
join_ssid#
uint8_t join_ssid[RSI_SSID_LEN]
Definition at line 1680
of file include/rsi_wlan.h
uRate#
uint8_t uRate
Definition at line 1681
of file include/rsi_wlan.h
uTxPower#
uint8_t uTxPower
Definition at line 1682
of file include/rsi_wlan.h
reserved_1#
uint8_t reserved_1
Definition at line 1683
of file include/rsi_wlan.h
reserved_2#
uint8_t reserved_2
Definition at line 1684
of file include/rsi_wlan.h
scan_ssid_len#
uint8_t scan_ssid_len
Definition at line 1685
of file include/rsi_wlan.h
reserved_3#
uint8_t reserved_3
Definition at line 1686
of file include/rsi_wlan.h
csec_mode#
uint8_t csec_mode
Definition at line 1687
of file include/rsi_wlan.h
psk#
uint8_t psk[RSI_PSK_LEN]
Definition at line 1688
of file include/rsi_wlan.h
scan_ssid#
uint8_t scan_ssid[RSI_SSID_LEN]
Definition at line 1689
of file include/rsi_wlan.h
scan_cnum#
uint8_t scan_cnum
Definition at line 1690
of file include/rsi_wlan.h
dhcp_enable#
uint8_t dhcp_enable
Definition at line 1691
of file include/rsi_wlan.h
uint8_t ip[IP_ADDRESS_SZ]
Definition at line 1692
of file include/rsi_wlan.h
sn_mask#
uint8_t sn_mask[IP_ADDRESS_SZ]
Definition at line 1693
of file include/rsi_wlan.h
dgw#
uint8_t dgw[IP_ADDRESS_SZ]
Definition at line 1694
of file include/rsi_wlan.h
eap_method#
uint8_t eap_method[32]
Definition at line 1695
of file include/rsi_wlan.h
inner_method#
uint8_t inner_method[32]
Definition at line 1696
of file include/rsi_wlan.h
user_identity#
uint8_t user_identity[64]
Definition at line 1697
of file include/rsi_wlan.h
passwd#
uint8_t passwd[128]
Definition at line 1698
of file include/rsi_wlan.h
go_intent#
uint8_t go_intent[2]
Definition at line 1699
of file include/rsi_wlan.h
device_name#
uint8_t device_name[64]
Definition at line 1700
of file include/rsi_wlan.h
operating_channel#
uint8_t operating_channel[2]
Definition at line 1701
of file include/rsi_wlan.h
ssid_postfix#
uint8_t ssid_postfix[64]
Definition at line 1702
of file include/rsi_wlan.h
psk_key#
uint8_t psk_key[64]
Definition at line 1703
of file include/rsi_wlan.h
pmk#
uint8_t pmk[WISE_PMK_LEN]
Definition at line 1704
of file include/rsi_wlan.h
apconfig#
rsi_apconfig apconfig
Definition at line 1705
of file include/rsi_wlan.h
module_mac#
uint8_t module_mac[6]
Definition at line 1706
of file include/rsi_wlan.h
antenna_select#
uint8_t antenna_select[2]
Definition at line 1707
of file include/rsi_wlan.h
reserved_4#
uint8_t reserved_4[2]
Definition at line 1708
of file include/rsi_wlan.h
wep_key#
rsi_wepkey wep_key
Definition at line 1709
of file include/rsi_wlan.h
dhcp6_enable#
uint8_t dhcp6_enable[2]
Definition at line 1710
of file include/rsi_wlan.h
prefix_length#
uint8_t prefix_length[2]
Definition at line 1711
of file include/rsi_wlan.h
ip6#
uint8_t ip6[16]
Definition at line 1712
of file include/rsi_wlan.h
dgw6#
uint8_t dgw6[16]
Definition at line 1713
of file include/rsi_wlan.h
tcp_stack_used#
uint8_t tcp_stack_used
Definition at line 1714
of file include/rsi_wlan.h
bgscan_magic_code#
uint8_t bgscan_magic_code[2]
Definition at line 1715
of file include/rsi_wlan.h
bgscan_enable#
uint8_t bgscan_enable[2]
Definition at line 1716
of file include/rsi_wlan.h
bgscan_threshold#
uint8_t bgscan_threshold[2]
Definition at line 1717
of file include/rsi_wlan.h
rssi_tolerance_threshold
uint8_t rssi_tolerance_threshold[2]
Definition at line 1718
of file include/rsi_wlan.h
bgscan_periodicity#
uint8_t bgscan_periodicity[2]
Definition at line 1719
of file include/rsi_wlan.h
active_scan_duration#
uint8_t active_scan_duration[2]
Definition at line 1720
of file include/rsi_wlan.h
passive_scan_duration#
uint8_t passive_scan_duration[2]
Definition at line 1721
of file include/rsi_wlan.h
multi_probe#
uint8_t multi_probe
Definition at line 1722
of file include/rsi_wlan.h
chan_bitmap_magic_code#
uint8_t chan_bitmap_magic_code[2]
Definition at line 1723
of file include/rsi_wlan.h
scan_chan_bitmap_stored_2_4_GHz#
uint8_t scan_chan_bitmap_stored_2_4_GHz[4]
Definition at line 1724
of file include/rsi_wlan.h
scan_chan_bitmap_stored_5_GHz#
uint8_t scan_chan_bitmap_stored_5_GHz[4]
Definition at line 1725
of file include/rsi_wlan.h
roam_magic_code#
uint8_t roam_magic_code[2]
Definition at line 1726
of file include/rsi_wlan.h
roam_params_stored#
rsi_uRoamParams roam_params_stored
Definition at line 1727
of file include/rsi_wlan.h
rejoin_magic_code#
uint8_t rejoin_magic_code[2]
Definition at line 1728
of file include/rsi_wlan.h
rejoin_param_stored#
rsi_rejoin_params_t rejoin_param_stored
Definition at line 1729
of file include/rsi_wlan.h
region_request_from_host#
uint8_t region_request_from_host
Definition at line 1730
of file include/rsi_wlan.h
rsi_region_code_from_host#
uint8_t rsi_region_code_from_host
Definition at line 1731
of file include/rsi_wlan.h
region_code#
uint8_t region_code
Definition at line 1732
of file include/rsi_wlan.h
reserved_5#
uint8_t reserved_5[43]
Definition at line 1733
of file include/rsi_wlan.h
multicast_magic_code#
uint8_t multicast_magic_code[2]
Definition at line 1734
of file include/rsi_wlan.h
multicast_bitmap#
uint8_t multicast_bitmap[2]
Definition at line 1735
of file include/rsi_wlan.h
powermode_magic_code#
uint8_t powermode_magic_code[2]
Definition at line 1736
of file include/rsi_wlan.h
powermode#
uint8_t powermode
Definition at line 1737
of file include/rsi_wlan.h
ulp_mode#
uint8_t ulp_mode
Definition at line 1738
of file include/rsi_wlan.h
wmm_ps_magic_code#
uint8_t wmm_ps_magic_code[2]
Definition at line 1739
of file include/rsi_wlan.h
wmm_ps_enable#
uint8_t wmm_ps_enable
Definition at line 1740
of file include/rsi_wlan.h
wmm_ps_type#
uint8_t wmm_ps_type
Definition at line 1741
of file include/rsi_wlan.h
wmm_ps_wakeup_interval#
uint8_t wmm_ps_wakeup_interval[4]
Definition at line 1742
of file include/rsi_wlan.h
wmm_ps_uapsd_bitmap#
uint8_t wmm_ps_uapsd_bitmap
Definition at line 1743
of file include/rsi_wlan.h
listen_interval#
uint8_t listen_interval[4]
Definition at line 1744
of file include/rsi_wlan.h
listen_interval_dtim#
uint8_t listen_interval_dtim
Definition at line 1745
of file include/rsi_wlan.h
ext_custom_feature_bit_map#
uint8_t ext_custom_feature_bit_map[4]
Definition at line 1746
of file include/rsi_wlan.h
private_key_password#
uint8_t private_key_password[82]
Definition at line 1747
of file include/rsi_wlan.h
join_bssid#
uint8_t join_bssid[6]
Definition at line 1748
of file include/rsi_wlan.h
join_feature_bitmap#
uint8_t join_feature_bitmap
Definition at line 1749
of file include/rsi_wlan.h
ht_caps#
rsi_uHtCaps ht_caps
Definition at line 1750
of file include/rsi_wlan.h
ht_caps_magic_word#
uint8_t ht_caps_magic_word[2]
Definition at line 1751
of file include/rsi_wlan.h
fast_psp_enable#
uint8_t fast_psp_enable
Definition at line 1752
of file include/rsi_wlan.h
monitor_interval#
uint8_t monitor_interval[2]
Definition at line 1753
of file include/rsi_wlan.h
request_timeout_magic_word#
uint8_t request_timeout_magic_word[2]
Definition at line 1754
of file include/rsi_wlan.h
timeout_value#
uint8_t timeout_value[2]
Definition at line 1755
of file include/rsi_wlan.h
timeout_bitmap#
uint8_t timeout_bitmap[4]
Definition at line 1756
of file include/rsi_wlan.h
dhcp_ap_enable#
uint8_t dhcp_ap_enable
Definition at line 1758
of file include/rsi_wlan.h
ap_ip#
uint8_t ap_ip[4]
Definition at line 1759
of file include/rsi_wlan.h
ap_sn_mask#
uint8_t ap_sn_mask[4]
Definition at line 1760
of file include/rsi_wlan.h
ap_dgw#
uint8_t ap_dgw[4]
Definition at line 1761
of file include/rsi_wlan.h
dhcp6_ap_enable#
uint8_t dhcp6_ap_enable[2]
Definition at line 1762
of file include/rsi_wlan.h
ap_prefix_length#
uint8_t ap_prefix_length[2]
Definition at line 1763
of file include/rsi_wlan.h
ap_ip6#
uint8_t ap_ip6[16]
Definition at line 1764
of file include/rsi_wlan.h
ap_dgw6#
uint8_t ap_dgw6[16]
Definition at line 1765
of file include/rsi_wlan.h
ext_tcp_ip_feature_bit_map#
uint8_t ext_tcp_ip_feature_bit_map[4]
Definition at line 1766
of file include/rsi_wlan.h
http_credentials_avail#
uint8_t http_credentials_avail
Definition at line 1767
of file include/rsi_wlan.h
http_username#
uint8_t http_username[MAX_HTTP_SERVER_USERNAME]
Definition at line 1768
of file include/rsi_wlan.h
http_password#
uint8_t http_password[MAX_HTTP_SERVER_PASSWORD]
Definition at line 1769
of file include/rsi_wlan.h