You are viewing documentation for version:2.11.3Public Attributes#uint16_twlan_stateuint16_tchannel_numberuint8_tssiduint8_tmac_addressuint8_tsec_typeuint8_tpmkuint8_tipv4_addressuint8_tipv6_addressuint8_treserved1uint8_treserved2Public Attribute Documentation#wlan_state#uint16_t wlan_statechannel_number#uint16_t channel_numberssid#uint8_t ssid[RSI_SSID_LEN]mac_address#uint8_t mac_address[6]sec_type#uint8_t sec_typepmk#uint8_t pmk[64]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]reserved1#uint8_t reserved1[2]reserved2#uint8_t reserved2[2]