Public Attributes#
Public Attribute Documentation#
transmit_enable#
uint8_t transmit_enable
Enables/disables the ble per transmit mode
1 PER Transmit Enable
0 PER Transmit Disable
phy_rate#
uint8_t phy_rate
Phy rate at which packets are transmitted
1 1Mbps
2 2 Mbps
4 125 Kbps Coded
8 500 Kbps Coded
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening.
In order to enable, one should give the scrambler seed value which is used on the receive side
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel)
0x00 Advertise Channel
0x01 Data Channel (to be used by Default)
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used
0 No Hopping
1 Fixed Hopping
2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna.
2 ONBOARD_ANT_SEL
3 EXT_ANT_SEL
rf_type#
uint8_t rf_type
Selection of RF type (internal/external)
BIT[7:6] - RECT selection for BLR (Default value -> 0b00)
BIT[5:4] - RECT selection for BLE 2 Mbps (Default value -> 0b00)
BIT[3:2] - RECT selection for BLE 1 Mbps (Default value -> 0b00)
BIT[1:0] - for rf_type(external - 0/internal - 1) (Default value -> 0b01) Note
The above macros are applicable for BLE
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used
2 BT_HP_CHAIN
3 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
pkt_len#
uint8_t pkt_len[2]
Length of the packet to be transmitted Max pkt_len to be transmitted is 255
payload_type#
uint8_t payload_type
Type of payload data sequence
0x00 PRBS9 sequence �11111111100000111101...
0x01 Repeated �11110000�
0x02 Repeated �10101010�
0x03 PRBS15
0x04 Repeated �11111111�
0x05 Repeated �00000000�
0x06 Repeated '00001111'
0x07 Repeated '01010101'
tx_power#
uint8_t tx_power
Transmit Power
This field corresponds to the transmit power. The range for the Tx Power Index is 1 to 63 (0 and 32 are invalid.)
If rf chain is BT_HP_CHAIN
1 - 12 BLE - HP Mode
127 magic number for selecting maximum possible power output
If rf chain is BT_LP_CHAIN
1 - 31 BLE - 0 dBm Mode
33 - 63 BLE- 10 dBm Mode
transmit_mode#
uint8_t transmit_mode
Transmit mode to be used either Burst/Continuous
0 BURST_MODE
1 CONTINUOUS_MODE
2 CONTINUOUS_WAVE_MODE (CW_MODE)
inter_pkt_gap#
uint8_t inter_pkt_gap
This field takes the value of inter packet gap.
Number of slots to be skipped between two packets - Each slot will be 1250usec
num_pkts#
uint8_t num_pkts[4]
This field defines the number of packets to be transmitted, default to zero for continuous transmission