Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

cfg_enable#

uint8_t cfg_enable

opermode#

uint8_t opermode[4]

feature_bit_map#

uint8_t feature_bit_map[4]

tcp_ip_feature_bit_map#

uint8_t tcp_ip_feature_bit_map[4]

custom_feature_bit_map#

uint8_t custom_feature_bit_map[4]

band#

uint8_t band

scan_feature_bitmap#

uint8_t scan_feature_bitmap

join_ssid#

uint8_t join_ssid[RSI_SSID_LEN]

uRate#

uint8_t uRate

uTxPower#

uint8_t uTxPower

reserved_1#

uint8_t reserved_1

reserved_2#

uint8_t reserved_2

scan_ssid_len#

uint8_t scan_ssid_len

reserved_3#

uint8_t reserved_3

csec_mode#

uint8_t csec_mode

psk#

uint8_t psk[RSI_PSK_LEN]

scan_ssid#

uint8_t scan_ssid[RSI_SSID_LEN]

scan_cnum#

uint8_t scan_cnum

dhcp_enable#

uint8_t dhcp_enable

ip#

uint8_t ip[IP_ADDRESS_SZ]

sn_mask#

uint8_t sn_mask[IP_ADDRESS_SZ]

dgw#

uint8_t dgw[IP_ADDRESS_SZ]

eap_method#

uint8_t eap_method[32]

inner_method#

uint8_t inner_method[32]

user_identity#

uint8_t user_identity[64]

passwd#

uint8_t passwd[128]

go_intent#

uint8_t go_intent[2]

device_name#

uint8_t device_name[64]

operating_channel#

uint8_t operating_channel[2]

ssid_postfix#

uint8_t ssid_postfix[64]

psk_key#

uint8_t psk_key[64]

pmk#

uint8_t pmk[WISE_PMK_LEN]

apconfig#

rsi_apconfig apconfig

module_mac#

uint8_t module_mac[6]

antenna_select#

uint8_t antenna_select[2]

reserved_4#

uint8_t reserved_4[2]

wep_key#

rsi_wepkey wep_key

dhcp6_enable#

uint8_t dhcp6_enable[2]

prefix_length#

uint8_t prefix_length[2]

ip6#

uint8_t ip6[16]

dgw6#

uint8_t dgw6[16]

tcp_stack_used#

uint8_t tcp_stack_used

bgscan_magic_code#

uint8_t bgscan_magic_code[2]

bgscan_enable#

uint8_t bgscan_enable[2]

bgscan_threshold#

uint8_t bgscan_threshold[2]

rssi_tolerance_threshold#

uint8_t rssi_tolerance_threshold[2]

bgscan_periodicity#

uint8_t bgscan_periodicity[2]

active_scan_duration#

uint8_t active_scan_duration[2]

passive_scan_duration#

uint8_t passive_scan_duration[2]

multi_probe#

uint8_t multi_probe

chan_bitmap_magic_code#

uint8_t chan_bitmap_magic_code[2]

scan_chan_bitmap_stored_2_4_GHz#

uint8_t scan_chan_bitmap_stored_2_4_GHz[4]

scan_chan_bitmap_stored_5_GHz#

uint8_t scan_chan_bitmap_stored_5_GHz[4]

roam_magic_code#

uint8_t roam_magic_code[2]

roam_params_stored#

rsi_uRoamParams roam_params_stored

rejoin_magic_code#

uint8_t rejoin_magic_code[2]

rejoin_param_stored#

rsi_rejoin_params_t rejoin_param_stored

region_request_from_host#

uint8_t region_request_from_host

rsi_region_code_from_host#

uint8_t rsi_region_code_from_host

region_code#

uint8_t region_code

reserved_5#

uint8_t reserved_5[43]

multicast_magic_code#

uint8_t multicast_magic_code[2]

multicast_bitmap#

uint8_t multicast_bitmap[2]

powermode_magic_code#

uint8_t powermode_magic_code[2]

powermode#

uint8_t powermode

ulp_mode#

uint8_t ulp_mode

wmm_ps_magic_code#

uint8_t wmm_ps_magic_code[2]

wmm_ps_enable#

uint8_t wmm_ps_enable

wmm_ps_type#

uint8_t wmm_ps_type

wmm_ps_wakeup_interval#

uint8_t wmm_ps_wakeup_interval[4]

wmm_ps_uapsd_bitmap#

uint8_t wmm_ps_uapsd_bitmap

listen_interval#

uint8_t listen_interval[4]

listen_interval_dtim#

uint8_t listen_interval_dtim

ext_custom_feature_bit_map#

uint8_t ext_custom_feature_bit_map[4]

private_key_password#

uint8_t private_key_password[82]

join_bssid#

uint8_t join_bssid[6]

join_feature_bitmap#

uint8_t join_feature_bitmap

ht_caps#

rsi_uHtCaps ht_caps

ht_caps_magic_word#

uint8_t ht_caps_magic_word[2]

fast_psp_enable#

uint8_t fast_psp_enable

monitor_interval#

uint8_t monitor_interval[2]

request_timeout_magic_word#

uint8_t request_timeout_magic_word[2]

timeout_value#

uint8_t timeout_value[2]

timeout_bitmap#

uint8_t timeout_bitmap[4]

dhcp_ap_enable#

uint8_t dhcp_ap_enable

ap_ip#

uint8_t ap_ip[4]

ap_sn_mask#

uint8_t ap_sn_mask[4]

ap_dgw#

uint8_t ap_dgw[4]

dhcp6_ap_enable#

uint8_t dhcp6_ap_enable[2]

ap_prefix_length#

uint8_t ap_prefix_length[2]

ap_ip6#

uint8_t ap_ip6[16]

ap_dgw6#

uint8_t ap_dgw6[16]

ext_tcp_ip_feature_bit_map#

uint8_t ext_tcp_ip_feature_bit_map[4]

http_credentials_avail#

uint8_t http_credentials_avail

http_username#

uint8_t http_username[MAX_HTTP_SERVER_USERNAME]

http_password#

uint8_t http_password[MAX_HTTP_SERVER_PASSWORD]