You are viewing documentation for version:2.11.5Public Attributes#uint8_tset_region_code_from_user_cmduint8_tcountry_codeuint8_tno_of_rulesuint8_tfirst_channeluint8_tno_of_channelsuint8_tmax_tx_powerstruct rsi_req_set_region_ap_s::@2channel_infoPublic Attribute Documentation#set_region_code_from_user_cmd#uint8_t set_region_code_from_user_cmdcountry_code#uint8_t country_code[RSI_COUNTRY_CODE_LENGTH]no_of_rules#uint8_t no_of_rules[4]first_channel#uint8_t first_channelno_of_channels#uint8_t no_of_channelsmax_tx_power#uint8_t max_tx_powerchannel_info#struct rsi_req_set_region_ap_s::@2 channel_info[RSI_MAX_POSSIBLE_CHANNEL]