Public Attributes#
Public Attribute Documentation#
receive_enable#
uint8_t receive_enable
Enables/disables the ble per receive mode
1 PER Receive Enable
0 PER Receive Disable
phy_rate#
uint8_t phy_rate
Phy rate at which packets are received
1 1Mbps
2 2 Mbps
4 125 Kbps Coded
8 500 Kbps Coded
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening.
In order to enable, one should give the scrambler seed value which is used on the transmit side
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel)
0x00 Advertise Channel
0x01 Data Channel (to be used by Default)
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used
0 No Hopping
1 Fixed Hopping
2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna.
2 ONBOARD_ANT_SEL
3 EXT_ANT_SEL
rf_type#
uint8_t rf_type
Selection of RF type (internal/external)
0 BT_EXTERNAL_RF
1 BT_INTERNAL_RF (to be used by Default) Note
The above macros are applicable for both BT and BLE
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used
2 BT_HP_CHAIN
3 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
ext_data_len_indication#
uint8_t ext_data_len_indication
This field enables/disables the extended data length
0 Extended Data length disabled (27 Bytes)
1 Extended Data length enabled (255 Bytes)
loop_back_mode#
uint8_t loop_back_mode
This field defines the loopback to be enable or disable
0 LOOP_BACK_MODE_DISABLE
1 LOOP_BACK_MODE_ENABLE
duty_cycling_en#
uint8_t duty_cycling_en
This field enables/disables the duty cycling
0 Duty Cycling Disabled (to be used by Default)
1 Duty Cycling Enabled