You are viewing documentation for version:2.12Public Attributes#uint8_twake_durationuint8_twake_duration_toluint8_twake_int_expuint8_twake_int_exp_toluint16_twake_int_mantissauint16_twake_int_mantissa_toluint8_timplicit_twtuint8_tun_announced_twtuint8_ttriggered_twtuint8_twake_duration_unituint8_ttwt_channeluint8_ttwt_protectionuint8_trestrict_tx_outside_tspuint8_ttwt_retry_limituint8_ttwt_retry_intervaluint8_treq_typePublic Attribute Documentation#wake_duration#uint8_t wake_durationwake_duration_tol#uint8_t wake_duration_tolwake_int_exp#uint8_t wake_int_expwake_int_exp_tol#uint8_t wake_int_exp_tolwake_int_mantissa#uint16_t wake_int_mantissawake_int_mantissa_tol#uint16_t wake_int_mantissa_tolimplicit_twt#uint8_t implicit_twtun_announced_twt#uint8_t un_announced_twttriggered_twt#uint8_t triggered_twtwake_duration_unit#uint8_t wake_duration_unittwt_channel#uint8_t twt_channeltwt_protection#uint8_t twt_protectionrestrict_tx_outside_tsp#uint8_t restrict_tx_outside_tsptwt_retry_limit#uint8_t twt_retry_limittwt_retry_interval#uint8_t twt_retry_intervalreq_type#uint8_t req_type