You are viewing documentation for version:2.13.0Public Attributes#uint8_tinquiry_typeuint8_tdev_addruint8_tname_lengthuint8_tremote_device_nameuint8_tcodint8_trssiPublic Attribute Documentation#inquiry_type#uint8_t inquiry_typeInquiry scan type dev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]remote device address name_length#uint8_t name_lengthName length of the remote device remote_device_name#uint8_t remote_device_name[RSI_DEV_NAME_LEN]Name of remote device with max length of 50 bytes cod#uint8_t cod[3]Class of Device rssi#int8_t rssiRSSI of the remote device