You are viewing documentation for version:2.13.0Public Attributes#uint32_tbeacon_lost_countuint32_tbeacon_rx_countuint32_tmcast_rx_countuint32_tmcast_tx_countuint32_tucast_rx_countuint32_tucast_tx_countuint32_toverrun_countPublic Attribute Documentation#beacon_lost_count#uint32_t beacon_lost_countbeacon_rx_count#uint32_t beacon_rx_countmcast_rx_count#uint32_t mcast_rx_countmcast_tx_count#uint32_t mcast_tx_countucast_rx_count#uint32_t ucast_rx_countucast_tx_count#uint32_t ucast_tx_countoverrun_count#uint32_t overrun_count