You are viewing documentation for version:2.13.1Public Attributes#void *serv_handleruint16_thandleuint16_tconfig_bitmapuuid_tatt_uuiduint8_tpropertyuint16_tdata_lenuint8_tdataPublic Attribute Documentation#serv_handler#void* serv_handlerservice handler handle#uint16_t handleAttribute handle config_bitmap#uint16_t config_bitmapatt_uuid#uuid_t att_uuidAttribute type UUID property#uint8_t propertyAttribute property data_len#uint16_t data_lenAttribute data length data#uint8_t data[RSI_DEV_ATT_LEN]Attribute data. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro