You are viewing documentation for version:2.13.1Public Attributes#uint16_twlan_stateuint16_tchannel_numberuint8_tssiduint8_tmac_addressuint8_tsec_typeuint8_tpmkuint8_tipv4_addressuint8_tipv6_addressuint8_tbssidPublic Attribute Documentation#wlan_state#uint16_t wlan_statechannel_number#uint16_t channel_numberssid#uint8_t ssid[RSI_SSID_LEN]mac_address#uint8_t mac_address[6]sec_type#uint8_t sec_typepmk#uint8_t pmk[64]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]bssid#uint8_t bssid[6]