You are viewing documentation for version:2.14.0PDFPublic Attributes#uint8_tip_versionuint8_tsock_descuint8_tsrc_portuint8_tdst_portuint8_tipv4_addressuint8_tipv6_addressunion rsi_cert_recv_s::@31ip_addressuint8_tsequence_nouint8_ttotal_lenuint8_tcurrent_lenuint8_tmore_chunksuint8_treservedPublic Attribute Documentation#ip_version#uint8_t ip_version[2]sock_desc#uint8_t sock_desc[2]src_port#uint8_t src_port[2]dst_port#uint8_t dst_port[2]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]ip_address#union rsi_cert_recv_s::@31 ip_addresssequence_no#uint8_t sequence_no[2]total_len#uint8_t total_len[2]current_len#uint8_t current_len[2]more_chunks#uint8_t more_chunksreserved#uint8_t reserved[5]