You are viewing documentation for version:2.14.1 (latest)Public Attributes#uint8_tdev_addruint8_tcurrent_modeuint8_treserveduint16_tmode_intervalPublic Attribute Documentation#dev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]remote device address current_mode#uint8_t current_modeIndicates the current state of connection between the local device and the remote device i.e., Active mode / Hold mode/ Sniff mode 0 ? Active Mode 1 ? Hold Mode 2 ? Sniff Mode reserved#uint8_t reservedReserved field for future use mode_interval#uint16_t mode_intervalThis specifies the time interval to each mode