Public Attributes#

uint32_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

clock#

uint32_t clock

LMAC timer BT Clock


Definition at line 472 of file include/rsi_bt_apis.h

tx_poll#

uint16_t tx_poll

Num of TXed POLLS


Definition at line 476 of file include/rsi_bt_apis.h

tx_null#

uint16_t tx_null

Num of TXed NULLS


Definition at line 479 of file include/rsi_bt_apis.h

rx_poll#

uint16_t rx_poll

Num of RXed POLLS


Definition at line 482 of file include/rsi_bt_apis.h

rx_null#

uint16_t rx_null

Num of RXed NULLS


Definition at line 485 of file include/rsi_bt_apis.h

dm1_pkt#

uint16_t dm1_pkt[2]

dm1_pkt[0] - Num of TXed dm1 Pkts dm1_pkt[1] - Num of RXed dm1 Pkts


Definition at line 489 of file include/rsi_bt_apis.h

dm3_pkt#

uint16_t dm3_pkt[2]

dm3_pkt[0] - Num of TXed dm3 Pkts dm3_pkt[1] - Num of RXed dm3 Pkts


Definition at line 493 of file include/rsi_bt_apis.h

dm5_pkt#

uint16_t dm5_pkt[2]

dm5_pkt[0] - Num of TXed dm5 Pkts dm5_pkt[1] - Num of RXed dm5 Pkts


Definition at line 497 of file include/rsi_bt_apis.h

dh1_pkt#

uint16_t dh1_pkt[2]

dh1_pkt[0] - Num of TXed dh1 Pkts dh1_pkt[1] - Num of RXed dh1 Pkts


Definition at line 501 of file include/rsi_bt_apis.h

dh3_pkt#

uint16_t dh3_pkt[2]

dh3_pkt[0] - Num of TXed dh3 Pkts dh3_pkt[1] - Num of RXed dh3 Pkts


Definition at line 505 of file include/rsi_bt_apis.h

dh5_pkt#

uint16_t dh5_pkt[2]

dh5_pkt[0] - Num of TXed dh5 Pkts dh5_pkt[1] - Num of RXed dh5 Pkts


Definition at line 509 of file include/rsi_bt_apis.h

edr_2dh1_pkt#

uint16_t edr_2dh1_pkt[2]

2dh1_pkt[0] - Num of TXed 2dh1 Pkts 2dh1_pkt[1] - Num of RXed 2dh1 Pkts


Definition at line 514 of file include/rsi_bt_apis.h

edr_2dh3_pkt#

uint16_t edr_2dh3_pkt[2]

2dh3_pkt[0] - Num of TXed 2dh3 Pkts 2dh3_pkt[1] - Num of RXed 2dh3 Pkts


Definition at line 518 of file include/rsi_bt_apis.h

edr_2dh5_pkt#

uint16_t edr_2dh5_pkt[2]

2dh5_pkt[0] - Num of TXed 2dh5 Pkts 2dh5_pkt[1] - Num of RXed 2dh5 Pkts


Definition at line 522 of file include/rsi_bt_apis.h

edr_3dh1_pkt#

uint16_t edr_3dh1_pkt[2]

3dh1_pkt[0] - Num of TXed 3dh1 Pkts 3dh1_pkt[1] - Num of RXed 3dh1 Pkts


Definition at line 526 of file include/rsi_bt_apis.h

edr_3dh3_pkt#

uint16_t edr_3dh3_pkt[2]

3dh3_pkt[0] - Num of TXed 3dh3 Pkts 3dh3_pkt[1] - Num of RXed 3dh3 Pkts


Definition at line 530 of file include/rsi_bt_apis.h

edr_3dh5_pkt#

uint16_t edr_3dh5_pkt[2]

3dh5_pkt[0] - Num of TXed 3dh5 Pkts 3dh5_pkt[1] - Num of RXed 3dh5 Pkts


Definition at line 534 of file include/rsi_bt_apis.h

no_of_crc_fail#

uint16_t no_of_crc_fail

Num of CRC Failed Packets


Definition at line 538 of file include/rsi_bt_apis.h

no_of_retries#

uint16_t no_of_retries

Num of Retransmission Packets


Definition at line 541 of file include/rsi_bt_apis.h

no_of_hdr_err#

uint16_t no_of_hdr_err

Num of Header Error Packets


Definition at line 544 of file include/rsi_bt_apis.h

no_of_seq_repeat#

uint16_t no_of_seq_repeat

Num of Duplicate Packets Received (If previous sequence number is received again)


Definition at line 548 of file include/rsi_bt_apis.h

ack_delay#

uint16_t ack_delay[11]

Num of ack packets received with delay of 10ms to 100ms and more that 100ms 10 - ack_delay[10] ......... >100 - ack_delay[10]


Definition at line 552 of file include/rsi_bt_apis.h

ack_received#

uint16_t ack_received

Num of ACK packets Received


Definition at line 555 of file include/rsi_bt_apis.h

nak_received#

uint16_t nak_received

Num of NAK packets Received


Definition at line 558 of file include/rsi_bt_apis.h

no_of_rx_missed#

uint16_t no_of_rx_missed

Num of missed response packets in the RX Slot


Definition at line 561 of file include/rsi_bt_apis.h

no_of_rx_error#

uint16_t no_of_rx_error

Num of RXed error packets in the RX Slot


Definition at line 564 of file include/rsi_bt_apis.h

tx_attempts#

uint16_t tx_attempts

Num of TX Attempts


Definition at line 567 of file include/rsi_bt_apis.h

tx_done#

uint16_t tx_done

Number of Packets TXed on Air


Definition at line 570 of file include/rsi_bt_apis.h