Public Attribute Documentation#
maxtxoctets#
uint16_t maxtxoctets
maxtxoctets Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
maxtxtime#
uint16_t maxtxtime
maxtxtime Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
maxrxoctets#
uint16_t maxrxoctets
maxrxoctets Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
maxrxtime#
uint16_t maxrxtime
maxrxtime Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.