You are viewing documentation for version:2.8.0Public Attributes#uint8_tdev_addruint8_tatt_iduint8_tnbr_valsuint8_tvalsPublic Attribute Documentation#dev_addr#uint8_t dev_addr[6]remote device address att_id#uint8_t att_idID of the Attribute nbr_vals#uint8_t nbr_valsNumber of Values Present in the given att_id vals#uint8_t vals[AVRCP_MAX_APP_SUPP_ATT_VALS]Values List #define AVRCP_MAX_APP_SUPP_ATT_VALS 5