Public Attributes#

rsi_common_state_t
int32_t
rsi_mutex_handle_t
rsi_common_cmd_response_t
rsi_semaphore_handle_t
uint16_t
uint8_t *
rsi_puf_state_t
efuse_ipmu_t *
rsi_semaphore_handle_t
rsi_semaphore_handle_t
uint8_t

Public Attribute Documentation#

status#

volatile int32_t status

Definition at line 723 of file include/rsi_common.h

common_mutex#

rsi_mutex_handle_t common_mutex

Definition at line 726 of file include/rsi_common.h

expected_response#

rsi_common_cmd_response_t expected_response

Definition at line 729 of file include/rsi_common.h

common_sem#

rsi_semaphore_handle_t common_sem

Definition at line 732 of file include/rsi_common.h

common_tx_pool#

rsi_pkt_pool_t common_tx_pool

Definition at line 735 of file include/rsi_common.h

power_save#

rsi_power_save_t power_save

Definition at line 738 of file include/rsi_common.h

ps_coex_mode#

uint16_t ps_coex_mode

Definition at line 741 of file include/rsi_common.h

app_buffer#

uint8_t* app_buffer

Definition at line 744 of file include/rsi_common.h

app_buffer_length#

uint32_t app_buffer_length

Definition at line 747 of file include/rsi_common.h

puf_state#

volatile rsi_puf_state_t puf_state

Definition at line 751 of file include/rsi_common.h

ipmu_calib_data_cb#

efuse_ipmu_t* ipmu_calib_data_cb

Definition at line 754 of file include/rsi_common.h

common_card_ready_sem#

rsi_semaphore_handle_t common_card_ready_sem

Definition at line 757 of file include/rsi_common.h

wakeup_gpio_sem#

rsi_semaphore_handle_t wakeup_gpio_sem

Definition at line 760 of file include/rsi_common.h

Referenced by rsi_req_wakeup , and rsi_driver_deinit

sync_mode#

uint8_t sync_mode

Definition at line 762 of file include/rsi_common.h

sl_fw_log_callback#

void(* sl_fw_log_callback) (uint8_t *log_message, uint16_t log_message_length)

Definition at line 764 of file include/rsi_common.h