You are viewing documentation for version:2.9.1Public Attributes#uint8_tdev_addruint8_thandleuint8_toffsetuint8_tlengthuint8_tatt_valuePublic Attribute Documentation#dev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]remote device address handle#uint8_t handle[2]attribute handle offset#uint8_t offset[2]attribute value offset length#uint8_t lengthlength of attribute value att_value#uint8_t att_value[RSI_DEV_ATT_LEN]This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro