Value of one of the 3 types (128 bit, 32 bit or 16 bit) of UUIDs.

Public Attributes#

uuid32_t
uuid16_t

Public Attribute Documentation#

val128#

uuid128_t val128

uint8_t[16], 128 bit(16 byte) UUID value


Definition at line 382 of file include/rsi_ble_apis.h

val32#

uuid32_t val32

uint8_t[4], 32 bit(4 bytes) UUID value


Definition at line 384 of file include/rsi_ble_apis.h

val16#

uuid16_t val16

uint8_t[2], 16 bit(2 bytes) UUID value


Definition at line 386 of file include/rsi_ble_apis.h