Public Attributes#

rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
int32_t
uint32_t

timer flag

rsi_device_state_t

Public Attribute Documentation#

rom_version_info#

uint32_t rom_version_info

Definition at line 923 of file include/rsi_common.h

tx_mask_event#

uint32_t tx_mask_event

Definition at line 924 of file include/rsi_common.h

tx_mutex#

rsi_mutex_handle_t tx_mutex

Definition at line 925 of file include/rsi_common.h

logging_mutex#

rsi_mutex_handle_t logging_mutex

Definition at line 927 of file include/rsi_common.h

debug_prints_mutex#

rsi_mutex_handle_t debug_prints_mutex

Definition at line 930 of file include/rsi_common.h

nwk_sem#

rsi_semaphore_handle_t nwk_sem

Definition at line 932 of file include/rsi_common.h

wlan_cmd_sem#

rsi_semaphore_handle_t wlan_cmd_sem

Definition at line 933 of file include/rsi_common.h

common_cmd_sem#

rsi_semaphore_handle_t common_cmd_sem

Definition at line 934 of file include/rsi_common.h

common_cmd_send_sem#

rsi_semaphore_handle_t common_cmd_send_sem

Definition at line 935 of file include/rsi_common.h

crypto_cmd_sem#

rsi_semaphore_handle_t crypto_cmd_sem

Definition at line 937 of file include/rsi_common.h

wlan_cmd_send_sem#

rsi_semaphore_handle_t wlan_cmd_send_sem

Definition at line 939 of file include/rsi_common.h

nwk_cmd_send_sem#

rsi_semaphore_handle_t nwk_cmd_send_sem

Definition at line 940 of file include/rsi_common.h

send_data_sem#

rsi_semaphore_handle_t send_data_sem

Definition at line 941 of file include/rsi_common.h

nwk_wait_bitmap#

uint8_t nwk_wait_bitmap

Definition at line 942 of file include/rsi_common.h

wlan_wait_bitmap#

uint8_t wlan_wait_bitmap

Definition at line 943 of file include/rsi_common.h

send_wait_bitmap#

uint8_t send_wait_bitmap

Definition at line 944 of file include/rsi_common.h

common_wait_bitmap#

uint8_t common_wait_bitmap

Definition at line 945 of file include/rsi_common.h

crypto_wait_bitmap#

uint8_t crypto_wait_bitmap

Definition at line 947 of file include/rsi_common.h

zigb_wait_bitmap#

uint8_t zigb_wait_bitmap

Definition at line 949 of file include/rsi_common.h

bt_wait_bitmap#

uint8_t bt_wait_bitmap

Definition at line 950 of file include/rsi_common.h

bt_cmd_wait_bitmap#

uint8_t bt_cmd_wait_bitmap

Definition at line 951 of file include/rsi_common.h

nwk_cmd_state#

volatile uint8_t nwk_cmd_state

Definition at line 952 of file include/rsi_common.h

nwk_status#

volatile int32_t nwk_status

Definition at line 953 of file include/rsi_common.h

socket_state#

volatile uint8_t socket_state

Definition at line 954 of file include/rsi_common.h

socket_status#

volatile int32_t socket_status

Definition at line 955 of file include/rsi_common.h

wlan_cmd_state#

volatile uint8_t wlan_cmd_state

Definition at line 956 of file include/rsi_common.h

common_cmd_state#

volatile uint8_t common_cmd_state

Definition at line 957 of file include/rsi_common.h

timer_counter#

volatile uint32_t timer_counter

Definition at line 958 of file include/rsi_common.h

driver_timer_start#

volatile uint32_t driver_timer_start

Definition at line 960 of file include/rsi_common.h

timer_start#

rsi_timer_instance_t timer_start

Definition at line 961 of file include/rsi_common.h

driver_rx_timer_start#

volatile uint32_t driver_rx_timer_start

Definition at line 964 of file include/rsi_common.h

rx_timer_start#

rsi_timer_instance_t rx_timer_start

Definition at line 965 of file include/rsi_common.h

rsi_spiTimer1#

uint32_t rsi_spiTimer1

Definition at line 969 of file include/rsi_common.h

rsi_spiTimer2#

uint32_t rsi_spiTimer2

Definition at line 970 of file include/rsi_common.h

rsi_spiTimer3#

uint32_t rsi_spiTimer3

Definition at line 971 of file include/rsi_common.h

rsi_spiTimer4#

uint32_t rsi_spiTimer4

Definition at line 972 of file include/rsi_common.h

rsi_sdioTimer#

uint32_t rsi_sdioTimer

Definition at line 975 of file include/rsi_common.h

sdio_read_buff#

uint8_t sdio_read_buff[SDIO_BUFFER_LENGTH]

Definition at line 978 of file include/rsi_common.h

non_pref_chan_read_buff#

char non_pref_chan_read_buff[RSI_SINGLE_NON_PREF_CHAN_PARAMS_LEN *RSI_MAX_POSSIBLE_SINGLE_BAND_CHANNEL]

Definition at line 981 of file include/rsi_common.h

rx_driver_flag#

uint32_t rx_driver_flag

timer flag


Definition at line 984 of file include/rsi_common.h

device_state#

volatile rsi_device_state_t device_state

Definition at line 985 of file include/rsi_common.h

rsi_wait_timeout_handler_error_cb#

void(* rsi_wait_timeout_handler_error_cb) (int32_t status, uint32_t cmd_type)

Definition at line 988 of file include/rsi_common.h

nwk_app_buffer#

uint8_t* nwk_app_buffer

Definition at line 991 of file include/rsi_common.h

nwk_app_buffer_length#

uint32_t nwk_app_buffer_length

Definition at line 994 of file include/rsi_common.h

module_type_valid#

uint8_t module_type_valid

Definition at line 995 of file include/rsi_common.h

module_type_id#

uint8_t module_type_id

Definition at line 996 of file include/rsi_common.h