Public Attribute Documentation#

nwk_error_call_back_handler#

void(* nwk_error_call_back_handler) (uint8_t command_type, uint32_t status, const uint8_t *buffer, const uint32_t length)

Definition at line 270 of file include/rsi_wlan_non_rom.h

http_client_response_handler#

void(* http_client_response_handler)(uint16_t status, const uint8_t *buffer, const uint16_t length, const uint32_t more_data)

Definition at line 277 of file include/rsi_wlan_non_rom.h

http_otaf_response_handler#

void(* http_otaf_response_handler) (uint16_t status, const uint8_t *buffer)

Definition at line 289 of file include/rsi_wlan_non_rom.h

rsi_sntp_client_create_response_handler#

void(* rsi_sntp_client_create_response_handler) (uint16_t status, const uint8_t cmd_type, const uint8_t *buffer)

Definition at line 292 of file include/rsi_wlan_non_rom.h

smtp_client_mail_response_handler#

void(* smtp_client_mail_response_handler) (uint16_t status, const uint8_t cmd_type)

Definition at line 295 of file include/rsi_wlan_non_rom.h

smtp_client_delete_response_handler#

void(* smtp_client_delete_response_handler) (uint16_t status, const uint8_t cmd_type)

Definition at line 298 of file include/rsi_wlan_non_rom.h

ftp_directory_list_call_back_handler#

void(* ftp_directory_list_call_back_handler) (uint16_t status, uint8_t *directory_list, uint16_t length, uint8_t end_of_list)

Definition at line 301 of file include/rsi_wlan_non_rom.h

ftp_file_read_call_back_handler#

void(* ftp_file_read_call_back_handler) (uint16_t status, uint8_t *file_content, uint16_t content_length, uint8_t end_of_file)

Definition at line 307 of file include/rsi_wlan_non_rom.h

data_transfer_complete_handler#

void(* data_transfer_complete_handler) (int32_t sockID, uint16_t length)

Definition at line 312 of file include/rsi_wlan_non_rom.h

rsi_webpage_request_handler#

void(* rsi_webpage_request_handler) (uint8_t type, uint8_t *url_name, uint8_t *post_content_buffer, uint32_t post_content_length, uint32_t status)

Definition at line 315 of file include/rsi_wlan_non_rom.h

rsi_json_object_update_handler#

void(* rsi_json_object_update_handler) (uint8_t *file_name, uint8_t *json_object, uint32_t length, uint32_t status)

Definition at line 322 of file include/rsi_wlan_non_rom.h

rsi_wireless_fw_upgrade_handler#

void(* rsi_wireless_fw_upgrade_handler) (uint8_t type, uint32_t status)

Definition at line 325 of file include/rsi_wlan_non_rom.h

rsi_json_object_event_handler#

void(* rsi_json_object_event_handler) (uint32_t status, uint8_t *json_object_str, uint32_t length)

Definition at line 328 of file include/rsi_wlan_non_rom.h

rsi_pop3_client_mail_response_handler#

void(* rsi_pop3_client_mail_response_handler) (uint16_t status, uint8_t cmd_type, const uint8_t *buffer)

Definition at line 331 of file include/rsi_wlan_non_rom.h

rsi_http_client_put_response_handler#

void(* rsi_http_client_put_response_handler) (uint16_t status, uint8_t cmd_type, const uint8_t *buffer, uint16_t length, const uint8_t end_of_put_pkt)

Definition at line 334 of file include/rsi_wlan_non_rom.h

rsi_http_client_post_data_response_handler#

void(* rsi_http_client_post_data_response_handler)(uint16_t status, const uint8_t *buffer, const uint16_t length, const uint32_t more_data)

Definition at line 342 of file include/rsi_wlan_non_rom.h

rsi_ota_fw_up_response_handler#

void(* rsi_ota_fw_up_response_handler) (uint16_t status, uint16_t chunk_number)

Definition at line 355 of file include/rsi_wlan_non_rom.h

rsi_dns_update_rsp_handler#

void(* rsi_dns_update_rsp_handler) (uint16_t status)

Definition at line 358 of file include/rsi_wlan_non_rom.h

rsi_dhcp_usr_cls_rsp_handler#

void(* rsi_dhcp_usr_cls_rsp_handler) (uint16_t status)

Definition at line 361 of file include/rsi_wlan_non_rom.h

rsi_emb_mqtt_remote_terminate_handler#

void(* rsi_emb_mqtt_remote_terminate_handler) (uint16_t status, uint8_t *buffer, const uint32_t length)

Definition at line 364 of file include/rsi_wlan_non_rom.h

rsi_emb_mqtt_publish_message_callback#

void(* rsi_emb_mqtt_publish_message_callback) (uint16_t status, uint8_t *buffer, const uint32_t length)

Definition at line 367 of file include/rsi_wlan_non_rom.h

rsi_emb_mqtt_keep_alive_timeout_callback#

void(* rsi_emb_mqtt_keep_alive_timeout_callback) (uint16_t status, uint8_t *buffer, const uint32_t length)

Definition at line 370 of file include/rsi_wlan_non_rom.h