Structure for rejoin_params

Public Attributes#

uint8_t

Scan interval in seconds between each retry.

uint8_t

Number of missed beacons that will trigger rejoin.

uint8_t

Retry enable or disable for first time joining.

Public Attribute Documentation#

rsi_max_try#

uint8_t rsi_max_try[4]

Maximum number of retries before indicating join failure
Note: A value of 1 indicates no retries, while 0 indicates infinite retries.


rsi_scan_interval#

uint8_t rsi_scan_interval[4]

Scan interval in seconds between each retry.


rsi_beacon_missed_count#

uint8_t rsi_beacon_missed_count[4]

Number of missed beacons that will trigger rejoin.


rsi_first_time_retry_enable#

uint8_t rsi_first_time_retry_enable[4]

Retry enable or disable for first time joining.