You are viewing documentation for version:2.14.0 (latest)PDFPublic Attributes#uint8_tip_versionuint8_tsocket_iduint8_tdest_portuint8_tipv4_addressuint8_tipv6_addressunion rsi_rsp_ltcp_est_s::@36dest_ip_addruint8_tmssuint8_twindow_sizeuint8_tsrc_port_numPublic Attribute Documentation#ip_version#uint8_t ip_version[2]socket_id#uint8_t socket_id[2]dest_port#uint8_t dest_port[2]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]dest_ip_addr#union rsi_rsp_ltcp_est_s::@36 dest_ip_addrmss#uint8_t mss[2]window_size#uint8_t window_size[4]src_port_num#uint8_t src_port_num[2]