Roaming Parameters set structure
Public Attributes#
uint8_t
uint8_t
Specifies the RSSI threshold (in dBm) below which the module will attempt to roam to a better access point.
uint8_t
Defines the hysteresis value to prevent frequent roaming when the RSSI fluctuates around the threshold.
struct rsi_uRoamParams::@43
uint8_t
Public Attribute Documentation#
roam_threshold#
uint8_t roam_threshold[4]
Specifies the RSSI threshold (in dBm) below which the module will attempt to roam to a better access point.
roam_hysteresis#
uint8_t roam_hysteresis[4]
Defines the hysteresis value to prevent frequent roaming when the RSSI fluctuates around the threshold.