Command Reference#

Running slt --help displays information about all available SLT commands.

Available Commands#

Command

Description

completion

Generate the autocompletion script for the specified shell.

daemon

Start or stop the SLT daemon.

download

Download package metadata. Supported for Conan packages only.

help

Display help information for any command.

install

Install a package.

launch

Launch the specified application UI by launch ID. Flags must be at the end of the command arguments.

list

List available packages.

locate

Locate installed packages, either globally or using a .slconf context.

running

Show running packages.

settings

Manage SLT settings.

uninstall

Uninstall a package.

update

Update installed packages.

where

Print the path to an installed package.