Simplicity Installer - Silicon Labs Tools (SLT) Version 1.1.0 (Jan 22, 2026) Release Notes#
Welcome to the General Availability (GA) Simplicity Installer - Silicon Labs Tool (SLT), used to install and manage the full Simplicity development environment, including Simplicity SDKs and tools.
Release Summary#
Key Features#
Added in 1.1.0#
Added support for package-based delivery of Simplicity SDK 2025.12 for Simplicity Studio 6.1 and SLC 6.0.15, as part of the migration from a monolithic to a modular SDK architecture.
Added Installer version information on main page.
Enhanced the uninstall command with the
--alloption, more descriptive help, and improved behavior when no IDs are specified.Improved package installation performance by enabling parallel downloads of Conan packages.
Bug Fixes#
Fixed in 1.1.0#
None
Chip Enablement#
This release supports Series 2 and Series 3 devices.
Removed/Deprecated Features#
None
Known Issues and Limitation#
UID | Issue or Limitation Description | Workaround (if any) |
|---|---|---|
Restricted Access Support: Early Access and Controlled Access installations are not supported in this release. | Contact Sales for Restricted Access content (Alpha or NDA restricted) | |
Studio Shortcut: Studio launch shortcut is only available on the desktop. | None | |
Installation path: The installation path for the Package Manager is not selectable by the user. | None | |
1594110 | An error may occur during a full installation, or when installing Commander using the Simplicity Studio UI or the SLT-CLI on Ubuntu systems, if the required bzip2 package is missing. | Install the missing dependency before running the Debian package installer: |
Additional Bug Fixes#
Fixed in Studio 1.1.0#
UID | Issue Description |
|---|---|
1564633 | Fixed installer failures during full Studio 6 installs when MinGW detection caused errors in the UI installer. |
1513272 | PSRIRT - H1 reported #3334163 The Simplicity Studio development platform has a command execution vulnerability. |