RAIL SDK Version 2.19.1 (July 21, 2025) - Release Notes#
Simplicity SDK Version 2025.6.1
The RAIL SDK is a complete software development suite for proprietary wireless applications. It was previously part of the Proprietary SDK. Starting with the RAIL SDK 2.18.0 release, Proprietary SDK is split into RAIL SDK and Connect SDK.
Silicon Labs RAIL (Radio Abstraction Interface Layer) is an intuitive and easily-customizable radio interface layer designed to support both proprietary and standards-based wireless protocols.
The RAIL SDK is supplied with extensive documentation and sample applications.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 2.19.1#
Underlying platform changes only.
Added in 2.19.0#
Upgraded all components and sample application to use RAIL 2.19.0.
API Changes#
Added in 2.19.1#
None.
Added in 2.19.0#
All API that used RAIL 2.18.x typedef returns or params have been updated to use RAIL 2.19.0.
unpack_packetgot a new parametersl_rail_handle_t rail_handle
Bug Fixes#
Fixed in 2.19.1#
None.
Fixed in 2.19.0#
Fixed the Mode Switch sample application default channel start and end values to follow standard.
Fixed issue that when sample application got the
receive 0command it only stopped the CLI print of the packet not the receiving.
Chip Enablement#
Added in 2.19.1#
None.
Added in 2.19.0#
EFRxG29
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 2.19.1#
None.
Added in 2.19.0#
sl_mainsupport instead of deprecatedsl_system, nowsl_mainwill provide themain.cfile in the root directory.RAIL 2.19.0 support, all APIs, variables, typedefs have been updated to follow the RAIL library changes. Some APIs have been changed to have newer versions with same functionality.
Enhancements#
Added in 2.19.1#
None.
Added in 2.19.0#
All sample application use sl_main instead of sl_system. main.c is now
provided by the platform component.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
Modified in 2.19.1#
None.
Modified in 2.19.0#
Old API | Modified |
|---|---|
uint16_t unpack_packet(uint8_t * rx_destination, const RAIL_RxPacketInfo_t * packet_information, uint8_t ** start_of_payload) | uint16_t unpack_packet(sl_rail_handle_t rail_handle, uint8_t *rx_destination, const sl_rail_rx_packet_info_t *packet_information, uint8_t **start_of_payload, phy_modulation_e modulation) |
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 2.19.1#
None.
Fixed in 2.19.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1424608 | Wrong default channel numbers in default radio configuration | None |
|
| 1375765 | CLI command `receive 0` only stopped the CLI print, not the receive. | None |
|
| 1426032 | Range Test remote Config did not work on boards without LCD support. | None |
|
Chip Enablement#
Added in 2.19.1#
None.
Added in 2.19.0#
| Chip Family | OPNs / Boards / OPN Combinations | Supported Software Variants (if applicable) | Supported Modes | Supported Host Interfaces |
|---|---|---|---|---|
| EFR32xG29 |
|
Standard |
|
SPI, EUSART, UART |
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
Modified in 2.19.1#
None.
Added in 2.19.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
| RAIL - SoC Energy Mod sample application |
|
Standard |
|
|
All |
Removed Examples#
None.
Deprecated Examples#
None.
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
| Change | Impact | Affected Software Variants if applicable | Affected Modes | Affected OPNs / Boards / OPN Combinations | Affected Host Interfaces |
|---|---|---|---|---|---|
|
Update of the unpack_packet |
|
Standard |
|
|
All |
Migration Guide#
Click here for the migration guide for deprecated, removed, and modified items.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1268208 | The power consumption of DK2600 can’t be optimized if configuration time for EM2 and if UART is being used, as the value of SL_IOSTREAM_USART_{instance}_BAUDRATE doesn’t take effect. The default value used instead is 115200 bps. Typical use case is RAIL - SoC Wireless M-bus Meter with DK2600 board. | None | Update UART baud rate to 9600 bps at Simplicity Studio Admin Console. This is necessary for EM2. |
|
| 1274248 | Range Test DMP instabilities in case of LTO. | None | Do not use LTO. |
|
| 1375450 | Wi-SUN HAN phys aren’t supported by Standard packet assembler and Packet Assistant components. | None | Do not use Wi-SUN HAN phys with RAIL SDK sample applications. |
|
| Updating the Baremetal sample applications to RTOS causes build errors. | None |
Follow the Platforms guide sl_main Baremetal to RTOS Application Transition |
|
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
RAIL SDK showcasing the usage of the RAIL library.
Compatible Software#
None.
Installation and Use#
To upgrade your existing software with this release, see instructions here.
To run your first demo, see our Getting Started Guides.
To kick start your development, see our Developer's Guide.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
To learn more about the software in this release, dive into our online documentation.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top ofthis page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.