New Features and Improvements#

This page covers all notable additions and new features for the Simplicity Studio Extension for VS Code.

Release 1.5.0#

  • Updated the extension’s Landing and Onboarding views with new getting started flows.

  • Refreshed the Simplicity Workspace with new Build, Flash, and Debug Toolbar, and new virtual folders for Binaries and Tools.

  • Added Devices Module to display connected devices.

  • Enabled integrated terminal support for VCOM, RTT, and SWO with a configuration page for terminal connections.

  • Introduced new Learn and Support Module.

  • Removed Silabs Quick Access view.

Release 1.4.0#

  • Added support for a Debug Configurator UI, where the debug configurations will be written into the project’s launch.json file.

  • Added SVD support from non-Studio source.

  • Extended extension setting with Logging Folder Path to easily find and/or modify the path where the VS Code extension collecting logs and svd files will be stored.

  • Added support for "Set setting to default" on VS Code command palette for users to revert setting changes.

  • Extended c_cpp_properties to include custom build configs.

  • Additional Sources were moved to a separate page out of the Build Configurator section. The new page includes option to add source files.

Release 1.3.1#

  • Production release of 1.3.0

Release [1.3.0-pre-release] - 2024-07-03#

  • Dedicated "Silicon Labs: Workspace" View

  • Support for Silicon Labs solutions, generated by Simplicity Studio - New Project Wizard

Release 1.2.0 - 2024-05-15#

  • Recover Silicon lab device command on device palette

  • Support flash 'bin' and 'rps' files to Silicon lab device

Release 1.1.0 - 2024-02-08#

  • Option for automatic build before flash action

  • Option for automatic build and flash before debug action

  • IP configuration for remote devices

Release 1.0.0 - 2023-12-06#

  • Production release