Known Issues#

Features Not Yet Implemented#

These features are currently under development or planned but not yet available in this Beta release.

Installer#

  • Restricted Access Support: Early Access and Controlled Access installation flows not yet supported.

  • Local SDK Extension Install: Manual installation of local SDK extensions is not currently available.

  • Standard OS Uninstall Support: Full uninstallation using native OS methods is not yet implemented.

Studio#

  • Multiple Instance Support: Running multiple instances of Studio simultaneously is not supported.

  • Ubuntu 24.04 Support: This OS version is not officially supported.

  • Matter Provisioning Tool: Not yet available in the current release.

Tools#

  • Tool Shortcuts Outside Studio: No standalone launcher shortcuts available for tools like Network Analyzer, Energy Profiler, etc.

Features Implemented but Not Fully Tested#

These features are available but have not yet completed full validation.

Studio#

  • macOS 14 (Sonoma): Preliminary support included. Some instability may occur.

Device Manager#

  • General Functionality: Feature set available but undergoing additional testing for robustness.

Tools#

For the following tools, functionality is present but may have performance, stability, or integration issues in edge cases.

  • AoA Analyzer

  • Channel Sounding Analyzer

  • Positioning Tool (Standalone)

  • AoA Viewer

  • Wi-Fi Commander

  • Wi-Fi Memory Estimator

  • Network Analyzer

  • Energy Profiler

  • Bluetooth NCP Commander

Known Bugs and Limitations#

Studio UI#

  • Device Selector Dialog: Limited filtering functionality by protocol.

  • Learn & Support: The User Guide link under Learn & Support incorrectly directs users to the Simplicity Studio v5 User Guide instead of the correct v6 User Guide.

Tools#

  • Device Manager

    • Capture functionality may not work as expected under certain conditions.

  • Windows BSOD with Older Adapter FW

    • Issue: A known issue can cause a Blue Screen of Death (BSOD) on Windows when using Simplicity Studio v6 or v5 with development boards running Adapter Firmware versions earlier than v2.0.0.

    • Recommendation: Update your development board to Adapter Firmware v2.0.0 or later, which is based on winUSB driver, to avoid this issue.

SDKs#

  • Amazon Sidewalk

    • Issue: Sample app project generation fails on Ubuntu 22.04.

    • Workaround: None currently available.

  • Z-Wave

    • Issue: Sample app project builds fail on all supported operating systems.

    • Workaround: Under investigation. Refer to the Z-Wave SDK release notes for updates.

  • Matter

    • Issue: Sample app project builds on Windows may fail due to excessively long path names (Windows MAX_PATH limitations).

    • Workaround: Use a shorter project directory path.