// Bluetooth LE//Version 4.0 //General ... Bluetooth Low Energy is a powerful and complex technology. ... with client/server, which are explained in GATT Server and Client Roles.
// Bluetooth LE//Version 5.0 //API Reference ... To use these new events, the application needs to include the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.
// Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... notification and scan requests will be reported as events. Default : 0 Enable or disable the scan request ...
Bluetooth LE and Bluetooth Mesh APIs have separate API reference manuals. ... cmd_gatt_write_descriptor_value | 0x09 | 0x0f | 4 | | Events | | evt_gatt_mtu_exchanged | 0x09 | 0x00 | 3 | | evt_ ...
... are often interested in the advertising payload that is 0-31 bytes long on the primary channels ... Bluetooth Core Specification - This is the golden reference, but not that easy to digest.