USB Device Vendor API
Description
USB Device Vendor API.
Data Structures | |
struct | sl_usbd_vendor_callbacks_t |
Vendor callbacks. |
Functions | |
sl_status_t | sl_usbd_vendor_init (void) |
Initialize the internal structures and variables used by the Vendor class. | |
sl_status_t | sl_usbd_vendor_create_instance (bool intr_en, uint16_t interval, sl_usbd_vendor_callbacks_t *p_vendor_callbacks, uint8_t *p_class_nbr) |
Add a new instance of the Vendor class. | |
sl_status_t | sl_usbd_vendor_add_to_configuration (uint8_t class_nbr, uint8_t config_nbr) |
Add the Vendor class instance into the specified configuration (see Note #1). | |
sl_status_t | sl_usbd_vendor_is_enabled (uint8_t class_nbr, bool *p_enabled) |
Get the vendor class enable state. | |
sl_status_t | sl_usbd_vendor_read_bulk_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len) |
Add a Microsoft OS extended property to this vendor class instance. | |
sl_status_t | sl_usbd_vendor_write_bulk_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, bool end, uint32_t *p_xfer_len) |
Send data to the host through Bulk IN endpoint. | |
sl_status_t | sl_usbd_vendor_read_bulk_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_vendor_async_function_t async_fnct, void *p_async_arg) |
Receive data from the host through the Bulk OUT endpoint. | |
sl_status_t | sl_usbd_vendor_write_bulk_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_vendor_async_function_t async_fnct, void *p_async_arg, bool end) |
Send data to the host through the Bulk IN endpoint. | |
sl_status_t | sl_usbd_vendor_read_interrupt_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len) |
Receive data from the the host through the Interrupt OUT endpoint. | |
sl_status_t | sl_usbd_vendor_write_interrupt_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, bool end, uint32_t *p_xfer_len) |
Send data to the host through the Interrupt IN endpoint. | |
sl_status_t | sl_usbd_vendor_read_interrupt_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_vendor_async_function_t async_fnct, void *p_async_arg) |
Receive data from the host through Interrupt OUT endpoint. | |
sl_status_t | sl_usbd_vendor_write_interrupt_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_vendor_async_function_t async_fnct, void *p_async_arg, bool end) |
Send data to the host through the Interrupt IN endpoint. |
Typedefs | |
typedef void(* | sl_usbd_vendor_async_function_t) (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status) |
App callback used for async comm. |
Function Documentation
◆ sl_usbd_vendor_init()
sl_status_t sl_usbd_vendor_init | ( | void |
| ) |
Initialize the internal structures and variables used by the Vendor class.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_create_instance()
sl_status_t sl_usbd_vendor_create_instance | ( | bool | intr_en, |
uint16_t | interval, |
||
sl_usbd_vendor_callbacks_t * | p_vendor_callbacks, |
||
uint8_t * | p_class_nbr |
||
) |
Add a new instance of the Vendor class.
- Parameters
-
intr_en
Interrupt endpoints IN and OUT flag: - true Pair of interrupt endpoints added to interface.
- false Pair of interrupt endpoints not added to interface.
interval
Endpoint interval in milliseconds (must be a power of 2). p_vendor_callbacks
Pointer to vendor callback structure. [Content MUST be persistent] p_class_nbr
Pointer to a variable that will receive class instance number, if no errors are returned, or SL_USBD_CLASS_NBR_NONE otherwise.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_add_to_configuration()
sl_status_t sl_usbd_vendor_add_to_configuration | ( | uint8_t | class_nbr, |
uint8_t | config_nbr |
||
) |
Add the Vendor class instance into the specified configuration (see Note #1).
- Parameters
-
class_nbr
Class instance number. config_nbr
Configuration index to which to add the Vendor class instance.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Called several times, it creates multiple instances and configurations. For instance, the following architecture could be created :
* FS * |-- Configuration 0 * |-- Interface 0 (Vendor 0) * |-- Configuration 1 * |-- Interface 0 (Vendor 0) * |-- Interface 1 (Vendor 1) *
In that example, there are two instances of Vendor class: 'Vendor 0' and '1', and two possible configurations: 'Configuration 0' and '1'. 'Configuration 1' is composed of two interfaces. Each class instance has an association with one of the interfaces. If 'Configuration 1' is activated by the host, it allows the host to access two different functionalities offered by the device. -
(2) Configuration Descriptor corresponding to a Vendor-specific device has the following format :
* Configuration Descriptor * |-- Interface Descriptor (Vendor class) * |-- Endpoint Descriptor (Bulk OUT) * |-- Endpoint Descriptor (Bulk IN) * |-- Endpoint Descriptor (Interrupt OUT) - optional * |-- Endpoint Descriptor (Interrupt IN) - optional *
◆ sl_usbd_vendor_is_enabled()
sl_status_t sl_usbd_vendor_is_enabled | ( | uint8_t | class_nbr, |
bool * | p_enabled |
||
) |
Get the vendor class enable state.
- Parameters
-
class_nbr
Class instance number. p_enabled
Pointer to a variable that will receive the enable state. The variable is set to true, if the Vendor class is enabled, and is set to false if the Vendor class is NOT enabled.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_read_bulk_sync()
sl_status_t sl_usbd_vendor_read_bulk_sync | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout, |
||
uint32_t * | p_xfer_len |
||
) |
Add a Microsoft OS extended property to this vendor class instance.
- Parameters
-
class_nbr
Class instance number. property_type
Property type (see Note #2). - OS_PROPERTY_TYPE_REG_SZ
- OS_PROPERTY_TYPE_REG_EXPAND_SZ
- OS_PROPERTY_TYPE_REG_BINARY
- OS_PROPERTY_TYPE_REG_DWORD_LITTLE_ENDIAN
- OS_PROPERTY_TYPE_REG_DWORD_BIG_ENDIAN
- OS_PROPERTY_TYPE_REG_LINK
- OS_PROPERTY_TYPE_REG_MULTI_SZ
p_property_name
Pointer to the buffer that contains the property name. -— Buffer assumed to be persistent -— property_name_len
Length of the property name in octets. p_property
Pointer to the buffer that contains the property name. -— Buffer assumed to be persistent -— property_len
Length of the property in octets.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) For more information on Microsoft OS descriptors, see 'http://msdn.microsoft.com/en-us/library/windows/hardware/gg463179.aspx'.
- (2) For more information on property types, refer to "Table 3. Property Data Types" of "Extended Properties OS Feature Descriptor Specification" document provided by Microsoft available at 'http://msdn.microsoft.com/en-us/library/windows/hardware/gg463179.aspx'.
Receive the data from the host through the Bulk OUT endpoint. This function is blocking.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the receive buffer. buf_len
Receive the buffer length in octets. timeout
Timeout in milliseconds. p_xfer_len
Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_write_bulk_sync()
sl_status_t sl_usbd_vendor_write_bulk_sync | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout, |
||
bool | end, |
||
uint32_t * | p_xfer_len |
||
) |
Send data to the host through Bulk IN endpoint.
This function is blocking.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the transmit buffer. buf_len
Transmit the buffer length in octets. timeout
Timeout in milliseconds. end
End-of-transfer flag (see Note #1). p_xfer_len
Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the end-of-transfer is set and the transfer length is a multiple of the maximum packet size, a zero-length packet is transferred to signal the end of transfer to the host.
◆ sl_usbd_vendor_read_bulk_async()
sl_status_t sl_usbd_vendor_read_bulk_async | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_vendor_async_function_t | async_fnct, |
||
void * | p_async_arg |
||
) |
Receive data from the host through the Bulk OUT endpoint.
This function is non-blocking are returns immediately after transfer preparation. Upon transfer completion, a callback provided by the application will be called to finalize the transfer.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the receive buffer. buf_len
Receive buffer length in octets. async_fnct
Receive the the callback. p_async_arg
Additional argument provided by the application for the receive callback.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_write_bulk_async()
sl_status_t sl_usbd_vendor_write_bulk_async | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_vendor_async_function_t | async_fnct, |
||
void * | p_async_arg, |
||
bool | end |
||
) |
Send data to the host through the Bulk IN endpoint.
This function is non-blocking and returns immediately after transfer preparation. Upon transfer completion, a callback provided by the application will be called to finalize the transfer.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the transmit buffer. buf_len
Transmit buffer length in octets. async_fnct
Transmit the callback. p_async_arg
Additional argument provided by the application for the transmit callback. end
End-of-transfer flag (see Note #1).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the end-of-transfer is set and the transfer length is a multiple of the maximum packet size, a zero-length packet is transferred to signal the end of transfer to the host.
◆ sl_usbd_vendor_read_interrupt_sync()
sl_status_t sl_usbd_vendor_read_interrupt_sync | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout, |
||
uint32_t * | p_xfer_len |
||
) |
Receive data from the the host through the Interrupt OUT endpoint.
This function is blocking.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the receive buffer. buf_len
Receive buffer length in octets. timeout
Timeout in milliseconds. p_xfer_len
Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_write_interrupt_sync()
sl_status_t sl_usbd_vendor_write_interrupt_sync | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout, |
||
bool | end, |
||
uint32_t * | p_xfer_len |
||
) |
Send data to the host through the Interrupt IN endpoint.
This function is blocking.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the transmit buffer. buf_len
Transmit buffer length in octets. timeout
Timeout in milliseconds. end
End-of-transfer flag (see Note #1). p_xfer_len
Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the end-of-transfer is set and the transfer length is a multiple of the maximum packet size, a zero-length packet is transferred to signal the end of transfer to the host.
◆ sl_usbd_vendor_read_interrupt_async()
sl_status_t sl_usbd_vendor_read_interrupt_async | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_vendor_async_function_t | async_fnct, |
||
void * | p_async_arg |
||
) |
Receive data from the host through Interrupt OUT endpoint.
This function is non-blocking and returns immediately after transfer preparation. Upon transfer completion, a callback provided by the application will be called to finalize the transfer.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the receive buffer. buf_len
Receive buffer length in octets. async_fnct
Receive callback. p_async_arg
Additional argument provided by application for the receive callback.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_vendor_write_interrupt_async()
sl_status_t sl_usbd_vendor_write_interrupt_async | ( | uint8_t | class_nbr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_vendor_async_function_t | async_fnct, |
||
void * | p_async_arg, |
||
bool | end |
||
) |
Send data to the host through the Interrupt IN endpoint.
This function is non-blocking and returns immediately after transfer preparation. Upon transfer completion, a callback provided by the application will be called to finalize the transfer.
- Parameters
-
class_nbr
Class instance number. p_buf
Pointer to the transmit buffer. buf_len
Transmit buffer length in octets. async_fnct
Transmit callback. p_async_arg
Additional argument provided by the application for the transmit callback. end
End-of-transfer flag (see Note #1).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the end-of-transfer is set and the transfer length is a multiple of the maximum packet size, a zero-length packet is transferred to signal the end of transfer to the host.
Typedef Documentation
◆ sl_usbd_vendor_async_function_t
typedef void(* sl_usbd_vendor_async_function_t) (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status) |
App callback used for async comm.