EFM32GG11: Micrium OS + LwIP Wi-Fi FMAC Driver Example

The WF200 Wi-Fi Expansion Board is the best and fastest way to explore the capabilities of the WF200 Series of Wi-Fi Transceivers. The kit contains an expansion board that can be connected to an EMF32 MCU starter-kit. The expansion board allows the EFM32 MCU to connect to a WF200 Wi-Fi module, which can connect to Wi-Fi networks, but also be an Access Point to which other devices can connect.

This document describes how to connect the WF200 Wi-Fi EXP Board to a GG11 MCU and run an HTTP Server example that toggles the LEDs.