Data Structures

Here are the data structures with brief descriptions:
HiCapabilities_tCapabilities offered by the WLAN used in command HiStartupIndBody_t
HiConfigurationCnfBody_tConfirmation message of CONFIGURATION command HiConfigurationReqBody_t
HiConfigurationReqBody_tConfigure the device
HiControlGpioCnfBody_tConfirmation from request to read and write a gpio
HiControlGpioReqBody_tSend a request to read or write a gpio identified by its label (that is defined in the PDS)
HiErrorIndBody_tError indication message
HiExceptionIndBody_tException indication message
HiGeneralCommandsIds_tGeneral command message IDs
HiGenericCnf_tGeneric confirmation message with the body reduced to the Status field
HiGenericIndBody_tGeneric indication message
HiGenericMsg_tGeneral message structure for all requests, confirmations and indications
HiMsgHdr_tGeneral Message header structure
HiOtpPhyInfo_tOTP_PHY_INFO OTP field reported in command HiStartupIndBody_t
HiOtpRegulSelModeInfo_tREGUL_SEL_MODE OTP field reported in command HiStartupIndBody_t
HiPreventRollbackCnfBody_tConfirmation of the Prevent Rollback request
HiPreventRollbackReqBody_tPrevent Rollback request
HiRxStats_tRX stats from the GENERIC indication message HiGenericIndBody_t
HiSetSlMacKeyCnfBody_tConfirmation for the Secure Link MAC key setting
HiSetSlMacKeyReqBody_tSet the Secure Link MAC key
HiSlConfigureCnfBody_tConfirmation of Secure Link Layer configuration HiSlConfigureReqBody_t
HiSlConfigureReqBody_tConfigure Secure Link Layer
HiSlExchangePubKeysCnfBody_tConfirmation for exchange of Secure Link Public Keys
HiSlExchangePubKeysReqBody_tExchange Secure Link Public Keys
HiStartupIndBody_tStartup Indication message
MsginfoBytes_t2 bytes view of the Message header information element
MsginfoUnion_tDifferent views of the Message header (HiMsgHdr_t) information element
wf200_basic_frame_tStructure used to describe the header of messages exchanged with wf200
wf200_buffer_tStructure used to describe the header of messages exchanged with wf200
wf200_context_tStructure used to maintain wf200 context on the host side
wf200_ethernet_frame_tStructure used to describe the ethernet frame exchanged with wf200
wf200_frame_tStructure used to describe the frame exchanged with wf200
WfmHiAddMulticastAddrCnf_tConfirmation message for WfmHiAddMulticastAddrReq_t
WfmHiAddMulticastAddrCnfBody_tConfirmation message body for WfmHiAddMulticastAddrCnf_t
WfmHiAddMulticastAddrReq_tRequest message for adding a multicast address to the multicast filter whitelist
WfmHiAddMulticastAddrReqBody_tRequest message body for WfmHiAddMulticastAddrReq_t
WfmHiApClientConnectedInd_tIndication message used to signal a connected station
WfmHiApClientConnectedIndBody_tIndication message body for WfmHiApClientConnectedInd_t
WfmHiApClientDisconnectedInd_tIndication message used to signal a disconnected station
WfmHiApClientDisconnectedIndBody_tIndication message body for WfmHiApClientDisconnectedInd_t
WfmHiApClientRejectedInd_tIndication message used to signal a rejected connection attempt from a station
WfmHiApClientRejectedIndBody_tIndication message body for WfmHiApClientRejectedInd_t
WfmHiConnectCnf_tConfirmation message for WfmHiConnectReq_t
WfmHiConnectCnfBody_tConfirmation message body for WfmHiConnectCnf_t
WfmHiConnectInd_tIndication message used to signal the completion of a connection operation
WfmHiConnectIndBody_tIndication message body for WfmHiConnectInd_t
WfmHiConnectReq_tRequest message for connecting to a Wi-Fi network
WfmHiConnectReqBody_tRequest message body for WfmHiConnectReq_t
WfmHiDisconnectApClientCnf_tConfirmation message for WfmHiDisconnectApClientReq_t
WfmHiDisconnectApClientCnfBody_tConfirmation message body for WfmHiDisconnectApClientCnf_t
WfmHiDisconnectApClientReq_tRequest message for disconnecting a client from the started Wi-Fi network
WfmHiDisconnectApClientReqBody_tRequest message body for WfmHiDisconnectApClientReq_t
WfmHiDisconnectCnf_tConfirmation message for WfmHiDisconnectReq_t
WfmHiDisconnectCnfBody_tConfirmation message body for WfmHiDisconnectCnf_t
WfmHiDisconnectInd_tIndication message used to signal the completion of a disconnection operation
WfmHiDisconnectIndBody_tIndication message body for WfmHiDisconnectInd_t
WfmHiDisconnectReq_tRequest message for disconnecting from a Wi-Fi network
WfmHiGetSignalStrengthCnf_tConfirmation message for WfmHiGetSignalStrengthReq_t
WfmHiGetSignalStrengthCnfBody_tConfirmation message body for WfmHiGetSignalStrengthCnf_t
WfmHiGetSignalStrengthReq_tRequest message for retrieving the signal strength of connection
WfmHiJoinIbssCnf_tConfirmation message for WfmHiJoinIbssReq_t
WfmHiJoinIbssCnfBody_tConfirmation message body for WfmHiJoinIbssCnf_t
WfmHiJoinIbssInd_tIndication message used to signal the completion of a join request
WfmHiJoinIbssIndBody_tIndication message body for WfmHiJoinIbssInd_t
WfmHiJoinIbssReq_tRequest message for connecting to or starting an IBSS network
WfmHiJoinIbssReqBody_tRequest message body for WfmHiJoinIbssReq_t
WfmHiLeaveIbssCnf_tConfirmation message for WfmHiLeaveIbssReq_t
WfmHiLeaveIbssCnfBody_tConfirmation message body for WfmHiLeaveIbssCnf_t
WfmHiLeaveIbssInd_tIndication message used to signal the completion of a disconnect operation
WfmHiLeaveIbssReq_tRequest message for disconnecting from an IBSS network
WfmHiNsIpAddr_tNS IP address element
WfmHiRateSetBitmask_tDevice TX rate set bitmask used in WfmHiSetTxRateParametersReqBody_t
WfmHiReceivedInd_tIndication message used to signal a received packet
WfmHiReceivedIndBody_tIndication message body for WfmHiReceivedInd_t
WfmHiRemoveMulticastAddrCnf_tConfirmation message for WfmHiRemoveMulticastAddrReq_t
WfmHiRemoveMulticastAddrCnfBody_tConfirmation message body for WfmHiRemoveMulticastAddrCnf_t
WfmHiRemoveMulticastAddrReq_tRequest message for removing a multicast address from the multicast filter whitelist
WfmHiRemoveMulticastAddrReqBody_tRequest message body for WfmHiRemoveMulticastAddrReq_t
WfmHiScanCompleteInd_tIndication message used to signal a scan was completed
WfmHiScanCompleteIndBody_tIndication message body for WfmHiScanCompleteInd_t
WfmHiScanResultInd_tIndication message used to signal an access point has been detected
WfmHiScanResultIndBody_tIndication message body for WfmHiScanResultInd_t
WfmHiSendFrameCnf_tConfirmation message for WfmHiSendFrameReq_t
WfmHiSendFrameCnfBody_tConfirmation message body for WfmHiSendFrameCnf_t
WfmHiSendFrameReq_tRequest message for sending a packet to the network
WfmHiSendFrameReqBody_tRequest message body for WfmHiSendFrameReq_t
WfmHiSetArpIpAddressCnf_tConfirmation message for WfmHiSetArpIpAddressReq_t
WfmHiSetArpIpAddressCnfBody_tConfirmation message body for WfmHiSetArpIpAddressCnf_t
WfmHiSetArpIpAddressReq_tRequest message for setting the Address Resolution Protocol (ARP) offloading state
WfmHiSetArpIpAddressReqBody_tRequest message body for WfmHiSetArpIpAddressReq_t
WfmHiSetBroadcastFilterCnf_tConfirmation message for WfmHiSetBroadcastFilterReq_t
WfmHiSetBroadcastFilterCnfBody_tConfirmation message body for WfmHiSetBroadcastFilterCnf_t
WfmHiSetBroadcastFilterReq_tRequest message for setting broadcast filter state
WfmHiSetBroadcastFilterReqBody_tRequest message body for WfmHiSetBroadcastFilterReq_t
WfmHiSetMacAddressCnf_tConfirmation message for WfmHiSetMacAddressReq_t
WfmHiSetMacAddressCnfBody_tConfirmation message body for WfmHiSetMacAddressCnf_t
WfmHiSetMacAddressReq_tRequest message to set MAC address of the interface
WfmHiSetMacAddressReqBody_tRequest message body for WfmHiSetMacAddressReq_t
WfmHiSetMaxApClientCountCnf_tConfirmation message for WfmHiSetMaxApClientCountReq_t
WfmHiSetMaxApClientCountCnfBody_tConfirmation message body for WfmHiSetMaxApClientCountCnf_t
WfmHiSetMaxApClientCountReq_tRequest message for setting the maximum number of connected clients
WfmHiSetMaxApClientCountReqBody_tRequest message body for WfmHiSetMaxApClientCountReq_t
WfmHiSetMaxApClientInactivityCnf_tConfirmation message for WfmHiSetMaxApClientInactivityReq_t
WfmHiSetMaxApClientInactivityCnfBody_tConfirmation message body for WfmHiSetMaxApClientCountCnf_t
WfmHiSetMaxApClientInactivityReq_tRequest message for setting the maximum number of connected clients
WfmHiSetMaxApClientInactivityReqBody_tRequest message body for WfmHiSetMaxApClientInactivityReq_t
WfmHiSetNsIpAddressCnf_tConfirmation message for WfmHiSetNsIpAddressReq_t
WfmHiSetNsIpAddressCnfBody_tConfirmation message body for WfmHiSetNsIpAddressCnf_t
WfmHiSetNsIpAddressReq_tRequest message for setting the Neighbor Discovery Protocol (NDP) offloading state
WfmHiSetNsIpAddressReqBody_tRequest message body for WfmHiSetNsIpAddressReq_t
WfmHiSetPmModeCnf_tConfirmation message for WfmHiSetPmModeReq_t
WfmHiSetPmModeCnfBody_tConfirmation message body for WfmHiSetPmModeCnf_t
WfmHiSetPmModeReq_tRequest message for setting the power management mode of the device
WfmHiSetPmModeReqBody_tRequest message body for WfmHiSetPmModeReq_t
WfmHiSetRoamParametersCnf_tConfirmation message for WfmHiSetRoamParametersReq_t
WfmHiSetRoamParametersCnfBody_tConfirmation message body for WfmHiSetRoamParametersCnf_t
WfmHiSetRoamParametersReq_tRequest message for setting the roaming parameters
WfmHiSetRoamParametersReqBody_tRequest message body for WfmHiSetRoamParametersReq_t
WfmHiSetScanParametersCnf_tConfirmation message for WfmHiSetScanParametersReq_t
WfmHiSetScanParametersCnfBody_tConfirmation message body for WfmHiSetScanParametersCnf_t
WfmHiSetScanParametersReq_tRequest message for setting scan parameters
WfmHiSetScanParametersReqBody_tRequest message body for WfmHiSetScanParametersReq_t
WfmHiSetTxRateParametersCnf_tConfirmation message for WfmHiSetTxRateParametersReq_t
WfmHiSetTxRateParametersCnfBody_tConfirmation message body for WfmHiSetTxRateParametersCnf_t
WfmHiSetTxRateParametersReq_tRequest message for setting the TX rate set parameters
WfmHiSetTxRateParametersReqBody_tRequest message body for WfmHiSetTxRateParametersReq_t
WfmHiSsidDef_tService Set Identifier (SSID) of a network
WfmHiStartApCnf_tConfirmation message for WfmHiStartApReq_t
WfmHiStartApCnfBody_tConfirmation message body for WfmHiStartApCnf_t
WfmHiStartApInd_tIndication message used to signal the completion of a start request
WfmHiStartApIndBody_tIndication message body for WfmHiStartApInd_t
WfmHiStartApReq_tRequest message for starting a Wi-Fi network
WfmHiStartApReqBody_tRequest message body for WfmHiStartApReq_t
WfmHiStartScanCnf_tConfirmation message for WfmHiStartScanReq_t
WfmHiStartScanCnfBody_tConfirmation message body for WfmHiStartScanCnf_t
WfmHiStartScanReq_tRequest message for starting a scan to detect near-by access points
WfmHiStartScanReqBody_tRequest message body for WfmHiStartScanReq_t
WfmHiStopApCnf_tConfirmation message for WfmHiStopApReq_t
WfmHiStopApCnfBody_tConfirmation message body for WfmHiStopApCnf_t
WfmHiStopApInd_tIndication message used to signal the completion of a stop operation
WfmHiStopApReq_tRequest message for stopping the started Wi-Fi network
WfmHiStopScanCnf_tConfirmation message for WfmHiStopScanReq_t
WfmHiStopScanCnfBody_tConfirmation message body for WfmHiStopScanCnf_t
WfmHiStopScanReq_tRequest message for stopping an ongoing scan
WfmHiUpdateApCnf_tConfirmation message for WfmHiUpdateApReq_t
WfmHiUpdateApCnfBody_tConfirmation message body for WfmHiUpdateApCnf_t
WfmHiUpdateApReq_tRequest message for updating parameters of the started Wi-Fi network
WfmHiUpdateApReqBody_tRequest message body for WfmHiUpdateApReq_t
WfmMessageIds_tWFM API message IDs