IBSS station state

WFM API messages applicable for an interface in IBSS mode.

Data Structures

struct  WfmHiSendFrameReq_t
 Request message for sending a packet to the network.
 
struct  WfmHiSendFrameCnf_t
 Confirmation message for WfmHiSendFrameReq_t.
 
struct  WfmHiReceivedInd_t
 Indication message used to signal a received packet.
 
struct  WfmHiLeaveIbssCnf_t
 Confirmation message for WfmHiLeaveIbssReq_t.
 
struct  WfmHiLeaveIbssReq_t
 Request message for disconnecting from an IBSS network.
 
struct  WfmHiLeaveIbssInd_t
 Indication message used to signal the completion of a disconnect operation.

Detailed Description

WFM API messages applicable for an interface in IBSS mode.


Data Structure Documentation

◆ WfmHiSendFrameReq_t

struct WfmHiSendFrameReq_t

Request message for sending a packet to the network.

The host can use this request to send a packet to the network.

Definition at line 1424 of file wfm_cmd_api.h.

Data Fields
WfmHiSendFrameReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSendFrameCnf_t

struct WfmHiSendFrameCnf_t

Confirmation message for WfmHiSendFrameReq_t.

Definition at line 1458 of file wfm_cmd_api.h.

Data Fields
WfmHiSendFrameCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiReceivedInd_t

struct WfmHiReceivedInd_t

Indication message used to signal a received packet.

The device will send this indication to signal a packet has been received.

Definition at line 1503 of file wfm_cmd_api.h.

Data Fields
WfmHiReceivedIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiLeaveIbssCnf_t

struct WfmHiLeaveIbssCnf_t

Confirmation message for WfmHiLeaveIbssReq_t.

Definition at line 1844 of file wfm_cmd_api.h.

Data Fields
WfmHiLeaveIbssCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiLeaveIbssReq_t

struct WfmHiLeaveIbssReq_t

Request message for disconnecting from an IBSS network.

The host can use this request to disconnect from an IBSS network.

Successful disconnect request moves the interface to Idle state.

◆ WfmHiLeaveIbssInd_t

struct WfmHiLeaveIbssInd_t

Indication message used to signal the completion of a disconnect operation.

The device will send this indication to signal the disconnect request initiated with WfmHiLeaveIbssReq_t has been completed. The indication is also sent when the network has encountered a fatal error.