App Notes#
The following upcoming application notes will provide information that is of interest to SiWx91x users developing with WiseConnect SDK v3.x.
Note: These application notes will be published soon. Stay tuned.
SiWx917 SoC Memory Map Application Note#
This application notes provides information about the memory regions of the SiWx917 such as random-access memory (RAM) and flash memory in order to facilitate optimized application design.
SiWx917 SoC Throughput Application Note#
This application note provides information about the SiWx917 chipset's throughput performance in System-on-chip (SoC) mode, where the application and connectivity stack run on the SiWx91x chipset. Information is also provided about the throughput over various network protocols like Transport Control Protocol (TCP), User Datagram Protocol (UDP), and Transport Layer Security (TLS).
SiWx917 SoC Low Power Application Note#
This application note provides information about the SiWx91x power save features in SoC mode, including current consumption values in the different power save modes and states. It also provides details on using the various power save examples in the WiSeConnect SDK v3.x.
SiWx917 SoC Firmware Update Application Note#
This application note provides information about the firmware update methods available in SoC mode.
SiWx917 NCP SPI Protocol Application Note#
This application note provides information on the hardware design and software configurations for the Serial Peripheral Interface (SPI) available in the SiWx91x chipset for operating in Network Co-processor (NCP) mode with external microcontroller unit (MCU) hosts, where the application runs on the external MCU host and the connectivity stack runs on the SiWx91x chipset.
SiWx917 NCP Low Power Application Note#
This application note provides information about the SiWx91x power save features in NCP mode, including current consumption values in the different power save modes and states. It also provides details on using the various power save examples in WiSeConnect SDK v3.x.
SiWx917 NCP Throughput Application Note#
This application notes provides information about the SiWx917 chipset's throughput performance in NCP mode, including throughput over various network protocols like Transport Control Protocol (TCP), User Datagram Protocol (UDP), and Transport Layer Security (TLS).
SiW917 NCP Firmware Update Application Note#
This application note provides information about the firmware update methods available in NCP mode.