Overview#

The SiWx91x™ chipset family runs the HyperText Transfer Protocol (HTTP) on its internal network processor and provides the ability for the application processor to exchange data with HTTP servers.

The WiSeConnect™ SDK v3.x provides an application programming interface (API) to access the HTTP features of the device.

The WiSeConnect™ SDK v3.x also provides an API to run the HyperText Transfer Protocol (HTTP) Server on its host processor. This facilitates the exchange of data between the client and server, enabling applications to handle and respond to HTTP requests.