WiSeConnect™ SDK Programming Guides#
This section provides guidance for developing applications using the WiSeConnect™ SDK. It contains the following guides:
Preprocessor Build Settings guide describes how to set values of common preprocessor macros.
Developing with Sockets guide describes writing applications for network communication with sockets.
Recommended Settings guide consolidates recommendations for both System-on-Chip (SoC) and Network Co-Processor (NCP) operation modes using the WiSeConnect™ SDK.
Power Manager guide describes how to implement requirement-based power management on SiWx917 SoC platforms.
Timer guide explains how to select and configure timer peripherals on SiWx917 devices.
Peripherals guide describes how to configure and use peripherals (such as the Generic Serial Peripheral Interface (GSPI), Inter-Integrated Circuit (I²C), Serial Synchronous Interface (SSI), Universal Asynchronous Receiver/Transmitter (UART), and Universal Synchronous/Asynchronous Receiver/Transmitter (USART)) on SiWx917 devices.
NVM and LittleFS guide describes how to configure and use the Little File System (LittleFS) and Non-Volatile Memory, Third Generation (NVM3) to manage memory on the SiWx917 platform.
SiWx917 Security Overview guide provides a summary of the security features of the SiWx917™.
SiWx917 Software Reference guide details the software architecture and programming features of the SiWx917.
Manufacturing Guides detail procedures for managing the hardware configuration, certificates, calibration, and other manufacturing settings of the SiWx917.