IP Communication#
This section provides guidelines to ping a Wi-SUN device from the Raspberry Pi running wsbrd. These guidelines assume that wsbrd has been configured and is running on the Raspberry Pi.
Ping and UDP: Detailed guidelines to ping the nodes after they are connected to the Border Router and perform UDP communication between using Netcat.
CoAP: Get the Wi-SUN Meter temperature and humidity values and control the boards LEDs using CoAP.
Wi-SUN Multicast: Silicon Labs Wi-SUN stack implements Multicast Protocol for Low-Power and Lossy Networks (MPL) as described in RFC7731, to support multicast packets messaging specified in the Wi-SUN FAN Technical Profile Specification version 1.1v06.