RPL parameter set.
Public Attributes#
uint16_t
RPL first DIS maximum delay (seconds)
uint16_t
RPL DIS maximum delay (seconds)
uint16_t
Delay for preferred parent selection after first DIO reception (seconds)
uint16_t
Maximum period of NS probes used to get samples for ETX calculation (seconds)
uint8_t
Number of samples used to calculate ETX during join state 4.
uint8_t
Number of samples used to refresh ETX.
uint8_t
RPL max candidate parents.
uint8_t
RPL max parents.
Public Attribute Documentation#
dis_max_delay_first_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_first_s
RPL first DIS maximum delay (seconds)
Definition at line
137
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
dis_max_delay_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_s
RPL DIS maximum delay (seconds)
Definition at line
139
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
init_parent_selection_s#
uint16_t sl_wisun_params_rpl::init_parent_selection_s
Delay for preferred parent selection after first DIO reception (seconds)
Definition at line
141
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_probe_period_max_s#
uint16_t sl_wisun_params_rpl::etx_probe_period_max_s
Maximum period of NS probes used to get samples for ETX calculation (seconds)
Definition at line
143
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_init#
uint8_t sl_wisun_params_rpl::etx_samples_init
Number of samples used to calculate ETX during join state 4.
Definition at line
145
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_refresh#
uint8_t sl_wisun_params_rpl::etx_samples_refresh
Number of samples used to refresh ETX.
Definition at line
147
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
candidate_parents_max#
uint8_t sl_wisun_params_rpl::candidate_parents_max
RPL max candidate parents.
Definition at line
149
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
parents_max#
uint8_t sl_wisun_params_rpl::parents_max
RPL max parents.
Definition at line
151
of file /mnt/raid/workspaces/ws.BCQzPo61M/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h