Prototype Phase#
This content contains recommended Z-Wave resources for development possibilities, and provides guidance on making basic customizations. As well as the content listed below, the Dr Z-Wave blog contains a lot of useful information and practices about Z-Wave technology and development. |
User Guides#
Name | Topic | Content |
|---|---|---|
ZAF | This document describes the Z-Wave Plus V2 Application Framework (ZAF), which is part of the Z-Wave SDK. The Application Framework delivers Command Class modules that can be reused between applications and also some additional modules that make it simpler to develop firmware for new Z-Wave products and devices. | |
Zniffer | Describes the Z-Wave Zniffer application, a development tool used for capturing Z-Wave RF communication and presenting the frames in a graphical user interface on a PC. | |
PC Controller | Describes the Z-Wave PC-based Controller application, a development tool used for communication with Z-Wave nodes through a Static Controller (SC). |
Associations#
Name | Topic | Content |
|---|---|---|
Association | Z-Wave Associations explained with the following content (16 min video): Theory, examples using PC Controller and Zniffer |
Long Range#
Name | Topic | Content |
|---|---|---|
Silicon Labs Z-Wave Training - LR Introduction (2 video presentations) | Long Range | Z-Wave Long Range Introduction + Sensor applications (30 min video) Z-Wave Long Range Hands-On Lab (26 min video) |
Long Range | Z-Wave Long Range Introduction + Sensor applications (30 min video) | |
Long Range | Z-Wave Long Range Hands-On Lab (26 min video) | |
Long Range | Knowledge article explaining how to set up Z-Wave Long Range with the Z-Wave 700 Starter Kit. |
700 Series#
Name | Topic | Content |
|---|---|---|
700 Series Timers | Knowledge article demonstrating an example of using a Software Timer to perform a temperature and humidity sensor reading once every second. It uses the AppTimer module from the Z-Wave Application Framework. | |
Z-Wave 700: How to implement I2C into the Z-Wave Embedded Framework | 700 Series I2C | Knowledge article showing how to interface to the Si7021 sensor using the I2C API from EMLIB and demonstrating how to get I2C implemented in the Z-Wave framework. The Si7021 Relative Humidity and Temperature Sensor used here is already mounted on the WSTK mainboard that is part of the Z-Wave 700 Development Kit. |
Z-Wave 700: How to implement SPI into the Z-Wave Embedded Framework | 700 Series SPI | Knowledge article showing an implementation of an SPI Master application. In order to implement SPI into the Z-Wave framework, it uses the SPIDRV API from EMDRV peripheral driver. |