Examples Overview#
This section contains:
- How to Use Certified Apps (PDF): Describes how to use the Z-Wave certified applications, which come as part of the Z-Wave SDK. The document explains the real-life application that a specific certified app is modelling, the Z-Wave specific configuration being used, and the functionality of buttons and LEDs on the expansion board. 
- How to Use Pre-Certified Apps (PDF): Describes how to use the Z-Wave pre-certified applications, which come as part of the Z-Wave SDK. They differ from the certified applications in that these applications are not formally certified but they do pass the CTT 3 test suite. The document explains the real-life application that a specific pre-certified app is modelling, the Z-Wave specific configuration being used, and the functionality of buttons and LEDs on the expansion board. 
Best Practices for Z-Wave Door Locks#
This multi-part series is written by Dr. ZWave, Eric Ryherd. It brings together the many issues unique to door locks and guides the developer toward the most robust and interoperable implementation. These are mostly recommendations, not requirements, and do not guarantee Z-Wave certification.